DatabaseAttributeManager Class¶
-
class
NXOpen.PDM.
DatabaseAttributeManager
¶ Bases:
NXOpen.TransientObject
This class is responsible for setting and getting NX Manager database attribute.
Use
PDM.PartBuilder.NewDatabaseAttributeManager
orPDM.PdmPart.NewDatabaseAttributeManager
to get the instance of this class.New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetAttribute | Gets the value of a writable database attribute. |
LoadAttributes | Load the Database Attributes from Teamcenter. |
LoadAttributesRecursively | Recursively load the Database Attributes of this part and all its partially or fully loaded components from Teamcenter. |
RefreshAttributes | Force load the Database Attributes from Teamcenter. |
SetAttribute | Sets the value of a writable database attribute. |
StoreAttributes | Register DB_PART_NAME and DB_PART_DESC attributes with values set in the attribute_manager |
Method Detail¶
Dispose¶
-
DatabaseAttributeManager.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetAttribute¶
-
DatabaseAttributeManager.
GetAttribute
¶ Gets the value of a writable database attribute.
Signature
GetAttribute(attributeTitle)
Parameters: attributeTitle (str) – the title of the attribute Returns: the value of the attribute Return type: str New in version NX4.0.0.
License requirements: None.
LoadAttributes¶
-
DatabaseAttributeManager.
LoadAttributes
¶ Load the Database Attributes from Teamcenter.
This operation will not discard any changes made in this session that aren’t committed to Teamcenter. If ‘reload’ is set to ‘true’, attributes that have already been loaded will be loaded again, if otherwise allowed.
Signature
LoadAttributes(reload)
Parameters: reload (bool) – Reload attributes that have already been loaded, if otherwise allowed. New in version NX8.0.0.
License requirements: None.
LoadAttributesRecursively¶
-
DatabaseAttributeManager.
LoadAttributesRecursively
¶ Recursively load the Database Attributes of this part and all its partially or fully loaded components from Teamcenter.
This operation will not discard any changes made in this session that aren’t committed to Teamcenter.
Signature
LoadAttributesRecursively(reload)
Parameters: reload (bool) – Reload attributes that have already been loaded, if otherwise allowed. New in version NX8.0.0.
License requirements: None.
RefreshAttributes¶
-
DatabaseAttributeManager.
RefreshAttributes
¶ Force load the Database Attributes from Teamcenter.
This removes changes to values made in NX.
Signature
RefreshAttributes()
New in version NX6.0.0.
License requirements: None.
SetAttribute¶
-
DatabaseAttributeManager.
SetAttribute
¶ Sets the value of a writable database attribute.
Signature
SetAttribute(attributeTitle, attributeValue)
Parameters: - attributeTitle (str) – the title of the attribute to be set
- attributeValue (str) – the new value the attribute is to be set to
New in version NX4.0.0.
License requirements: None.