NXOpen.Formboard Package¶
Classes¶
FaceAnnotationBuilder Class | Builder for Face Annotation functionality used in formboard. |
FlipComponentBuilder Class | Builder for flip component operation used in formboard. |
FormboardLayoutBuilder Class | Class that performs the layout of Formboard geometry. |
FormboardManager Class | Contains information about flattened harness drawing and drafting data for harness manufacturing drawings (Formboard Drawings). |
LayoutLengthOptions Class | Defines the various options for determining the rounded lengths of formboard geometry during the layout or update process. |
ObjectAttributeReferenceBuilder Class | Builder for object attribute used in formboard which enbles user to create annotation in drafting functionality. |
OrientBranchBuilder Class | Builder for Orient Branch operation used in formboard. |
PathLengthAnnotationBuilder Class | TODO Class documentation |
ShapeSegmentBuilder Class | Builder for Face Annotation functionality used in formboard. |
UpdateDiscrepancy Class | Defines a discrepancy object which contains information about a specific difference between the formboard drawing and the 3D harness model. |
UpdateFormboardBuilder Class | Class that performs the update of Formboard geometry. |
Enumerations¶
FaceAnnotationBuilderDrwDestination Enumeration | Enum which defines where the geometry is to be placed. |
FaceAnnotationBuilderTypes Enumeration | Enum which defines the type to import CGM/Pattern file |
FlipComponentBuilderAxisType Enumeration | Enum for the selection of axis type for flipping formboard component |
FormboardLayoutBuilderBranchAngle Enumeration | Methods for determining which angles to apply at each branch of the Formboard. |
FormboardLayoutBuilderBranchShape Enumeration | Shape option for the branches. |
FormboardLayoutBuilderMainRunType Enumeration | Selection method for the set of segments that define the main run of the formboard geometry. |
LayoutLengthOptionsRoundingMethod Enumeration | Methods of rounding lengths for Formboard geometry. |
ObjectAttributeReferenceBuilderLeaderType Enumeration | Enum which defines types of leader user wants to associate with the annotation. |
OrientBranchBuilderBranchAngleMethod Enumeration | Enum to define the type of method to orient branch. |
PathLengthAnnotationBuilderTypes Enumeration | TODO: Document the whole type |
UpdateDiscrepancyObjectType Enumeration | Specifies the type of objects involved in the discrepancy. |
UpdateDiscrepancyType Enumeration | The general type of the discrepancy. |