UpdateFormboardBuilder Class¶
-
class
NXOpen.Formboard.
UpdateFormboardBuilder
¶ Bases:
NXOpen.Builder
Class that performs the “update” of Formboard geometry.
To create a new instance of this class, use
NXOpen.Formboard.FormboardManager.CreateUpdateFormboardBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
LengthOptions | Returns the length options for the update operation. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateBendsOfRadialBends | Creates bends for radial bends after all discrepanices have been fixed. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DetermineDiscrepancies | Once the mapping has been determined, this method can find any discrepancies between the 3D harness and the formboard. |
FindMapping | Compute the mapping between the data in the formboard and the data in the 3D harness. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDiscrepancy | Returns the discrepancy at the given index. |
GetHarnessPart | Gets the 3D harness part file to compare the formboard against. |
GetNumberOfDiscrepancies | Returns the number of discrepancies discovered by the Formboard.UpdateFormboardBuilder.DetermineDiscrepancies() . |
GetObject | Returns the object currently being edited by this builder. |
RemoveBendsOfRadialBends | Removes bends in all radial bends and replaces them with a linear segment going from the anchor to the free RCP of each radial bend. |
SetHarnessPart | Sets the 3D harness part file to compare the formboard against. |
SetHarnesses | Sets the harnesses within the harness part that the formboard must be compared with. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LengthOptions¶
-
UpdateFormboardBuilder.
LengthOptions
¶ Returns the length options for the update operation.
-------------------------------------
Getter Method
Signature
LengthOptions
Returns: Return type: NXOpen.Formboard.LayoutLengthOptions
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
CreateBendsOfRadialBends¶
-
UpdateFormboardBuilder.
CreateBendsOfRadialBends
¶ Creates bends for radial bends after all discrepanices have been fixed.
This routine should be called in conjunction with RemoveBendsOfRadialBends.
Signature
CreateBendsOfRadialBends()
New in version NX7.5.5.
License requirements: routing_harness (“Routing Harness”)
DetermineDiscrepancies¶
-
UpdateFormboardBuilder.
DetermineDiscrepancies
¶ Once the mapping has been determined, this method can find any discrepancies between the 3D harness and the formboard.
Signature
DetermineDiscrepancies()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
FindMapping¶
-
UpdateFormboardBuilder.
FindMapping
¶ Compute the mapping between the data in the formboard and the data in the 3D harness.
This method can take a very long time to execute.
Signature
FindMapping()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
GetDiscrepancy¶
-
UpdateFormboardBuilder.
GetDiscrepancy
¶ Returns the discrepancy at the given index.
The index must be 0 to
Formboard.UpdateFormboardBuilder.GetNumberOfDiscrepancies()
.Signature
GetDiscrepancy(index)
Parameters: index (int) – Returns: Return type: NXOpen.Formboard.UpdateDiscrepancy
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
GetHarnessPart¶
-
UpdateFormboardBuilder.
GetHarnessPart
¶ Gets the 3D harness part file to compare the formboard against.
Signature
GetHarnessPart()
Returns: Return type: NXOpen.Part
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
GetNumberOfDiscrepancies¶
-
UpdateFormboardBuilder.
GetNumberOfDiscrepancies
¶ Returns the number of discrepancies discovered by the
Formboard.UpdateFormboardBuilder.DetermineDiscrepancies()
.Signature
GetNumberOfDiscrepancies()
Returns: Return type: int New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
RemoveBendsOfRadialBends¶
-
UpdateFormboardBuilder.
RemoveBendsOfRadialBends
¶ Removes bends in all radial bends and replaces them with a linear segment going from the anchor to the free RCP of each radial bend.
This is done before fixing discrepancies because presence of bends in radial bend causes problems. The bends of radial bends are recreated after the discrepancies have been fixed using CreateBendsOfRadialBends
Signature
RemoveBendsOfRadialBends()
New in version NX7.5.5.
License requirements: routing_harness (“Routing Harness”)
SetHarnessPart¶
-
UpdateFormboardBuilder.
SetHarnessPart
¶ Sets the 3D harness part file to compare the formboard against.
This clears any discrepancies that have been discovered against the previous harness part.
Signature
SetHarnessPart(harnessPart)
Parameters: harnessPart ( NXOpen.Part
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
SetHarnesses¶
-
UpdateFormboardBuilder.
SetHarnesses
¶ Sets the harnesses within the harness part that the formboard must be compared with.
Signature
SetHarnesses(harnesses)
Parameters: harnesses (list of NXOpen.Routing.Electrical.HarnessDevice
) – Harnesses to compare against.New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Validate¶
-
UpdateFormboardBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.