FaceAnnotationBuilderDrwDestination Enumeration¶
NXOpen.Formboard.FaceAnnotationBuilder.DrwDestination is an alias for NXOpen.Formboard.FaceAnnotationBuilderDrwDestination
-
class
NXOpen.Formboard.
FaceAnnotationBuilderDrwDestination
¶ Bases:
object
Enum which defines where the geometry is to be placed. The geometry can be placed either in model or drawing sheet.
Enum Members
Enum Member Enum Member Description DrawingSheet Place geometry in drawing sheet Model Place geometry in model -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-