FlipComponentBuilder Class¶
-
class
NXOpen.Formboard.
FlipComponentBuilder
¶ Bases:
NXOpen.Builder
Builder for flip component operation used in formboard.
Allows user to flip the component by 180 degrees about an axis which is orthogonal to Z axis so that after flipping , the component lies in XY plane.
To create a new instance of this class, use
NXOpen.Formboard.FormboardManager.CreateFlipComponentBuilder()
Default values.
Property Value AxisTypeEnum PathLocations New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AxisTypeEnum | Returns or sets the user selected NXOpen.Formboard.FlipComponentBuilderAxisType method |
CompSel | Returns the formboard component selected by user for flipping operation |
CustomAxis | Returns or sets the custom axis which is created when NXOpen.Formboard.FlipComponentBuilderAxisType is NXOpen.Formboard.FlipComponentBuilderAxisType.Custom |
PathAxisSel | Returns the axis selected by user about which selected formboard component will be flipped. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateDatumAxis | Creates datums axis at locations where selected formboard component is connected to path. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipComponent | Flips the selected formboard component by rotation angle about selected axis. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InitializeFromComponent | Initializes or resets ( start or stop ) drag operation based on the component selected for flipping operation. |
SetRotationAngle | Set the angle to rotate the component. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
StartDrag | Starts the drag operation of selected object. |
StopDrag | Stop the drag operation of selected object. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FlipComponentBuilderAxisType Enumeration | Enum for the selection of axis type for flipping formboard component |
Property Detail¶
AxisTypeEnum¶
-
FlipComponentBuilder.
AxisTypeEnum
¶ Returns or sets the user selected
NXOpen.Formboard.FlipComponentBuilderAxisType
method-------------------------------------
Getter Method
Signature
AxisTypeEnum
Returns: Return type: NXOpen.Formboard.FlipComponentBuilderAxisType
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
AxisTypeEnum
Parameters: axisTypeEnum ( NXOpen.Formboard.FlipComponentBuilderAxisType
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
CompSel¶
-
FlipComponentBuilder.
CompSel
¶ Returns the formboard component selected by user for flipping operation
-------------------------------------
Getter Method
Signature
CompSel
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
CustomAxis¶
-
FlipComponentBuilder.
CustomAxis
¶ Returns or sets the custom axis which is created when
NXOpen.Formboard.FlipComponentBuilderAxisType
isNXOpen.Formboard.FlipComponentBuilderAxisType.Custom
-------------------------------------
Getter Method
Signature
CustomAxis
Returns: Return type: NXOpen.Axis
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
CustomAxis
Parameters: customAxis ( NXOpen.Axis
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
PathAxisSel¶
-
FlipComponentBuilder.
PathAxisSel
¶ Returns the axis selected by user about which selected formboard component will be flipped.
-------------------------------------
Getter Method
Signature
PathAxisSel
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
CreateDatumAxis¶
-
FlipComponentBuilder.
CreateDatumAxis
¶ Creates datums axis at locations where selected formboard component is connected to path.
Signature
CreateDatumAxis()
Returns: Return type: list of NXOpen.NXObject
New in version NX4.0.0.
License requirements: routing_harness (“Routing Harness”)
FlipComponent¶
-
FlipComponentBuilder.
FlipComponent
¶ Flips the selected formboard component by rotation angle about selected axis.
Signature
FlipComponent()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
InitializeFromComponent¶
-
FlipComponentBuilder.
InitializeFromComponent
¶ Initializes or resets ( start or stop ) drag operation based on the component selected for flipping operation.
Signature
InitializeFromComponent()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
SetRotationAngle¶
-
FlipComponentBuilder.
SetRotationAngle
¶ Set the angle to rotate the component.
Signature
SetRotationAngle(angle)
Parameters: angle (float) – Rotation angle New in version NX7.5.3.
License requirements: routing_harness (“Routing Harness”)
StartDrag¶
-
FlipComponentBuilder.
StartDrag
¶ Starts the drag operation of selected object.
Does nothing if drag has already been started.
Signature
StartDrag()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
StopDrag¶
-
FlipComponentBuilder.
StopDrag
¶ Stop the drag operation of selected object.
Does nothing if drag has not been started.
Signature
StopDrag()
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Validate¶
-
FlipComponentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.