FlipComponentBuilderAxisType Enumeration¶
NXOpen.Formboard.FlipComponentBuilder.AxisType is an alias for NXOpen.Formboard.FlipComponentBuilderAxisType
-
class
NXOpen.Formboard.
FlipComponentBuilderAxisType
¶ Bases:
object
Enum for the selection of axis type for flipping formboard component
Enum Members
Enum Member Enum Member Description PathLocations Flip component by path locations Custom Flip component by user defined custom axis -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-