UpdateDiscrepancyObjectType Enumeration¶
NXOpen.Formboard.UpdateDiscrepancy.ObjectType is an alias for NXOpen.Formboard.UpdateDiscrepancyObjectType
-
class
NXOpen.Formboard.
UpdateDiscrepancyObjectType
¶ Bases:
object
Specifies the type of objects involved in the discrepancy.
Enum Members
Enum Member Enum Member Description Unknown Unknown type. Rcp Routing Control Point. Segment Routing Segment. Clip A component not assigned as a electrical connector. Component A component assigned as a electrical connector or device. Harness Harness. Wire Wire connection. Cable Cable connection. Shield Shield connection. Connector ConnectorDevice object which has a type of connector. Device ConnectorDevice object which has a type of device. Overstock Overstock. Fillerstock Filler stock. FittingOverstock Overstock applied to fittings. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-