ObjectAttributeReferenceBuilder Class¶
-
class
NXOpen.Formboard.
ObjectAttributeReferenceBuilder
¶ Bases:
NXOpen.Builder
Builder for “object attribute” used in formboard which enbles user to create annotation in drafting functionality.
It creates a tabular note and displays object attributes of a single object selected by user.
To create a new instance of this class, use
NXOpen.Formboard.FormboardManager.CreateObjectAttributeReferenceBuilder()
Default values.
Property Value EnumType None New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AnnotLeader | Returns the Annotations.LeaderBuilder for the annotation |
CompOrigin | Returns the comp origin |
EnumType | Returns or sets the enum type |
ObjectSelection | Returns the object selected by user to associated annotation |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ObjectAttributeReferenceBuilderLeaderType Enumeration | Enum which defines types of leader user wants to associate with the annotation. |
Property Detail¶
AnnotLeader¶
-
ObjectAttributeReferenceBuilder.
AnnotLeader
¶ Returns the
Annotations.LeaderBuilder
for the annotation-------------------------------------
Getter Method
Signature
AnnotLeader
Returns: Return type: NXOpen.Annotations.LeaderBuilder
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
CompOrigin¶
-
ObjectAttributeReferenceBuilder.
CompOrigin
¶ Returns the comp origin
-------------------------------------
Getter Method
Signature
CompOrigin
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
EnumType¶
-
ObjectAttributeReferenceBuilder.
EnumType
¶ Returns or sets the enum type
-------------------------------------
Getter Method
Signature
EnumType
Returns: Return type: NXOpen.Formboard.ObjectAttributeReferenceBuilderLeaderType
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
-------------------------------------
Setter Method
Signature
EnumType
Parameters: enumType ( NXOpen.Formboard.ObjectAttributeReferenceBuilderLeaderType
) –New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
ObjectSelection¶
-
ObjectAttributeReferenceBuilder.
ObjectSelection
¶ Returns the object selected by user to associated annotation
-------------------------------------
Getter Method
Signature
ObjectSelection
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: routing_harness (“Routing Harness”)
Method Detail¶
Validate¶
-
ObjectAttributeReferenceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.