OriginBuilder Class¶
-
class
NXOpen.Annotations.
OriginBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.OriginBuilder
This is a sub-builder class and cannot be directly instantiated
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Anchor | Returns or sets the anchor location of the origin on the annotation |
AnnotationView | Returns the view of the annotation (drafting member views only) |
Origin | Returns the origin |
OriginPoint | Returns or sets the origin point |
Plane | Returns the plane |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetAssociativeOrigin | Gets the data that specifies the origin’s associativity |
SetAssociativeOrigin | Associates the annotation’s origin to the specified objects |
SetInferRelativeToGeometry | Infers a relative to geometry associative on commit if no other associativity has been applied |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OriginBuilderAlignmentPosition Enumeration | alignment position on the annotation |
Property Detail¶
Anchor¶
-
OriginBuilder.
Anchor
¶ Returns or sets the anchor location of the origin on the annotation
-------------------------------------
Getter Method
Signature
Anchor
Returns: Return type: NXOpen.Annotations.OriginBuilderAlignmentPosition
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Anchor
Parameters: anchor ( NXOpen.Annotations.OriginBuilderAlignmentPosition
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”) OR solid_modeling (“SOLIDS MODELING”)
AnnotationView¶
-
OriginBuilder.
AnnotationView
¶ Returns the view of the annotation (drafting member views only)
-------------------------------------
Getter Method
Signature
AnnotationView
Returns: Return type: NXOpen.Drawings.SelectDraftingView
New in version NX6.0.0.
License requirements: None.
Origin¶
-
OriginBuilder.
Origin
¶ Returns the origin
-------------------------------------
Getter Method
Signature
Origin
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX6.0.0.
License requirements: None.
OriginPoint¶
-
OriginBuilder.
OriginPoint
¶ Returns or sets the origin point
-------------------------------------
Getter Method
Signature
OriginPoint
Returns: Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OriginPoint
Parameters: origin ( NXOpen.Point3d
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”) OR solid_modeling (“SOLIDS MODELING”)
Plane¶
-
OriginBuilder.
Plane
¶ Returns the plane
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.Annotations.PlaneBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetAssociativeOrigin¶
-
OriginBuilder.
GetAssociativeOrigin
¶ Gets the data that specifies the origin’s associativity
Signature
GetAssociativeOrigin()
Returns: associativity data Return type: NXOpen.Annotations.AnnotationAssociativeOriginData_Struct
New in version NX6.0.0.
License requirements: None.
SetAssociativeOrigin¶
-
OriginBuilder.
SetAssociativeOrigin
¶ Associates the annotation’s origin to the specified objects
Signature
SetAssociativeOrigin(assocOrigin)
Parameters: assocOrigin ( NXOpen.Annotations.AnnotationAssociativeOriginData_Struct
) – associativity dataNew in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”) OR solid_modeling (“SOLIDS MODELING”)
SetInferRelativeToGeometry¶
-
OriginBuilder.
SetInferRelativeToGeometry
¶ Infers a relative to geometry associative on commit if no other associativity has been applied
Signature
SetInferRelativeToGeometry(inferRelativeToGeometry)
Parameters: inferRelativeToGeometry (bool) – relative to geometry flag New in version NX6.0.1.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”) OR solid_modeling (“SOLIDS MODELING”)
Validate¶
-
OriginBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.