FormboardLayoutBuilderBranchAngle Enumeration¶
NXOpen.Formboard.FormboardLayoutBuilder.BranchAngle is an alias for NXOpen.Formboard.FormboardLayoutBuilderBranchAngle
-
class
NXOpen.Formboard.
FormboardLayoutBuilderBranchAngle
¶ Bases:
object
Methods for determining which angles to apply at each branch of the Formboard.
Enum Members
Enum Member Enum Member Description AsDesigned Use the angle equal to the 3D angle of the branch in the 3D harness. StandardAngles Apply a standard angle to the branch, the level of the branch determines which angle to apply. MaximumAngles Apply the largest possible angle values at every branch to force the harness to spread out. RandomAngles Randomly choose an angle for each branch. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-