UpdateDiscrepancyType Enumeration¶
NXOpen.Formboard.UpdateDiscrepancy.Type is an alias for NXOpen.Formboard.UpdateDiscrepancyType
-
class
NXOpen.Formboard.
UpdateDiscrepancyType
¶ Bases:
object
The general type of the discrepancy.
Enum Members
Enum Member Enum Member Description Unknown Unknown type, not valid. Missing Object exits in the 3D harness but is missing from the formboard. Extra Object is in the formboard but not in the 3D harness. Modified Object exists in both 3D and the formboard but is modified in some way. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-