FormboardLayoutBuilderMainRunType Enumeration¶
NXOpen.Formboard.FormboardLayoutBuilder.MainRunType is an alias for NXOpen.Formboard.FormboardLayoutBuilderMainRunType
-
class
NXOpen.Formboard.
FormboardLayoutBuilderMainRunType
¶ Bases:
object
Selection method for the set of segments that define the main run of the formboard geometry.
Enum Members
Enum Member Enum Member Description Longest Path of longest wire. Thickest Path of longest wire contained within the thickest bundle. UserSelection Manual selection of path. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-