AestheticFaceBlendBuilder Class¶
-
class
NXOpen.Features.
AestheticFaceBlendBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
This class will provide ability to create aesthetically pleasing blend surfaces on sheet and solid bodies.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateAestheticFaceBlendBuilder()
Default values.
Property Value AlignmentOption RollingBall BaseRadiusLaw.Function ft BaseRadiusLaw.LawType MultiTransition BaseRadiusLaw.Parameter t BlendFacesOption TrimtoAllInputFaces BlendOption Radius CenterChordLaw.LawType Constant CenterOption CenterRadius CenterRadiusLaw.LawType MultiTransition Chain1Continuity.ContinuityType G1 Chain2Continuity.ContinuityType G1 ChordLength.Value (deprecated) 10 (millimeters part), 0.4 (inches part) ChordLengthLaw.LawType Constant Continuity.ContinuityType (deprecated) G1 CurvatureTolerance 0.5 Degrees.Degree 3 Degrees.SegmentsOrPatches 1 Degrees.UDegree 5 Degrees.UPatches 1 Degrees.VDegree 5 Degrees.VPatches 1 IsAccelerated 1 IsBezier 0 IsCenterlineCurve 0 IsMinimumRadius 0 IsMinimumSubtendedAngle 0 IsRationalOutput 0 IsSameTransition 1 IsSewAllFaces 0 IsTrimInputFaces 0 IsWashout1 0 IsWashout2 0 MinimumEdgeLength 10 MinimumRadius.Value 2.5 (millimeters part), 0.098 (inches part) MinimumSubtendedAngle 5.0 RhoOption Relative RhoValue 0.6 SectionScaling1.Value 1 SectionScaling2.Value 1 SegmentationOption AtAllTransitions ShapeOption (deprecated) Accelerated New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AlignmentOption | Returns or sets the alignment option |
BaseRadiusLaw | Returns the base radius law variable |
BlendFacesOption | Returns or sets the blend faces option |
BlendOption | Returns or sets the method option |
CenterChordLaw | Returns the center chord law |
CenterOption | Returns or sets the center option |
CenterRadiusLaw | Returns the center radius law |
Chain1Continuity | Returns the chain 1 continuity |
Chain2Continuity | Returns the chain 2 continuity |
ChordLength | Returns the chord length |
ChordLengthLaw | Returns the chord length law variable |
ConstrainedEndPoint1 | Returns or sets the end point1 |
ConstrainedEndPoint2 | Returns or sets the end point2 |
ConstrainedStartPoint1 | Returns or sets the start point1 |
ConstrainedStartPoint2 | Returns or sets the start point2 |
Continuity | Returns the continuity |
CurvatureTolerance | Returns or sets the curvature tolerance |
Degrees | Returns the degrees |
FaceChain1 | Returns the face chain1 |
FaceChain2 | Returns the face chain2 |
IsAccelerated | Returns or sets the method to control the shape |
IsBezier | Returns or sets the bezier |
IsCenterlineCurve | Returns or sets the centerline curve |
IsMinimumRadius | Returns or sets the is min radius |
IsMinimumSubtendedAngle | Returns or sets the minimum subtended angle flag |
IsRationalOutput | Returns or sets the rational output |
IsSameTransition | Returns or sets the blend cross section is using the same transition as blend tangent or not |
IsSewAllFaces | Returns or sets the is sew faces |
IsTrimInputFaces | Returns or sets the is trim faces |
IsWashout1 | Returns or sets the washout1 |
IsWashout2 | Returns or sets the toggle washout2 |
LimitsList | Returns the trim object collector list |
MinimumEdgeLength | Returns or sets the max edge length |
MinimumRadius | Returns the min radius |
MinimumSubtendedAngle | Returns or sets the minimum subtended angle |
ParameterSpine | Returns the parameter spine |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PositionTolerance | Returns or sets the position tolerance |
RelativeEndBlendEndPoint | Returns or sets the relative end point on the washout curve of end blend. |
RelativeEndBlendStartPoint | Returns or sets the relative start point on the washout curve of end blend. |
RelativeStartBlendEndPoint | Returns or sets the relative end point on the washout curve of start blend. |
RelativeStartBlendStartPoint | Returns or sets the relative start point on the washout curve of start blend. |
ReverseNormal1 | Returns or sets the reverse normal1 |
ReverseNormal2 | Returns or sets the reverse normal2 |
RhoOption | Returns or sets the rho option |
RhoValue | Returns or sets the rho value |
SectionAlignmentVector | Returns or sets the section alignment vector |
SectionScaling1 | Returns the section scaling |
SectionScaling2 | Returns the section scaling2 |
SegmentationOption | Returns or sets the segmentation option |
ShapeOption | Returns or sets the shape option |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TangentMagnitude | Returns the tangent magnitude |
TangentTolerance | Returns or sets the tangent tolerance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AestheticFaceBlendBuilderAlignmentType Enumeration | Alignment method provides the ability to align the cross sections of the blend in the user specified direction |
AestheticFaceBlendBuilderBlendFacesType Enumeration | Trimming options |
AestheticFaceBlendBuilderBlendType Enumeration | Tangent method will create tangent lines based on the method employed. |
AestheticFaceBlendBuilderCenterType Enumeration | Center methods will define peak of the blend |
AestheticFaceBlendBuilderEndTrimObjectType Enumeration | End object overriding trim options |
AestheticFaceBlendBuilderRhoType Enumeration | Rho options |
AestheticFaceBlendBuilderSegmentationType Enumeration | Segmentations options |
AestheticFaceBlendBuilderShapeType Enumeration | Shape methods will define the high level shape of the blend cross section. |
AestheticFaceBlendBuilderStartTrimObjectType Enumeration | Start object overriding trim options |
Property Detail¶
AlignmentOption¶
-
AestheticFaceBlendBuilder.
AlignmentOption
¶ Returns or sets the alignment option
-------------------------------------
Getter Method
Signature
AlignmentOption
Returns: Return type: NXOpen.Features.AestheticFaceBlendBuilderAlignmentType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignmentOption
Parameters: alignmentOption ( NXOpen.Features.AestheticFaceBlendBuilderAlignmentType
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
BaseRadiusLaw¶
-
AestheticFaceBlendBuilder.
BaseRadiusLaw
¶ Returns the base radius law variable
-------------------------------------
Getter Method
Signature
BaseRadiusLaw
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX7.5.0.
License requirements: None.
BlendFacesOption¶
-
AestheticFaceBlendBuilder.
BlendFacesOption
¶ Returns or sets the blend faces option
-------------------------------------
Getter Method
Signature
BlendFacesOption
Returns: Return type: NXOpen.Features.AestheticFaceBlendBuilderBlendFacesType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlendFacesOption
Parameters: blendFacesOption ( NXOpen.Features.AestheticFaceBlendBuilderBlendFacesType
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
BlendOption¶
-
AestheticFaceBlendBuilder.
BlendOption
¶ Returns or sets the method option
-------------------------------------
Getter Method
Signature
BlendOption
Returns: Return type: NXOpen.Features.AestheticFaceBlendBuilderBlendType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlendOption
Parameters: blendOption ( NXOpen.Features.AestheticFaceBlendBuilderBlendType
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
CenterChordLaw¶
-
AestheticFaceBlendBuilder.
CenterChordLaw
¶ Returns the center chord law
-------------------------------------
Getter Method
Signature
CenterChordLaw
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX8.0.0.
License requirements: None.
CenterOption¶
-
AestheticFaceBlendBuilder.
CenterOption
¶ Returns or sets the center option
-------------------------------------
Getter Method
Signature
CenterOption
Returns: Return type: NXOpen.Features.AestheticFaceBlendBuilderCenterType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterOption
Parameters: centerOption ( NXOpen.Features.AestheticFaceBlendBuilderCenterType
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
CenterRadiusLaw¶
-
AestheticFaceBlendBuilder.
CenterRadiusLaw
¶ Returns the center radius law
-------------------------------------
Getter Method
Signature
CenterRadiusLaw
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX7.5.0.
License requirements: None.
Chain1Continuity¶
-
AestheticFaceBlendBuilder.
Chain1Continuity
¶ Returns the chain 1 continuity
-------------------------------------
Getter Method
Signature
Chain1Continuity
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX8.0.0.
License requirements: None.
Chain2Continuity¶
-
AestheticFaceBlendBuilder.
Chain2Continuity
¶ Returns the chain 2 continuity
-------------------------------------
Getter Method
Signature
Chain2Continuity
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX8.0.0.
License requirements: None.
ChordLength¶
-
AestheticFaceBlendBuilder.
ChordLength
¶ Returns the chord length
-------------------------------------
Getter Method
Signature
ChordLength
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
Features.AestheticFaceBlendBuilder.ChordLengthLaw()
instead.License requirements: None.
ChordLengthLaw¶
-
AestheticFaceBlendBuilder.
ChordLengthLaw
¶ Returns the chord length law variable
-------------------------------------
Getter Method
Signature
ChordLengthLaw
Returns: Return type: NXOpen.GeometricUtilities.LawBuilder
New in version NX8.0.0.
License requirements: None.
ConstrainedEndPoint1¶
-
AestheticFaceBlendBuilder.
ConstrainedEndPoint1
¶ Returns or sets the end point1
-------------------------------------
Getter Method
Signature
ConstrainedEndPoint1
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstrainedEndPoint1
Parameters: endPoint1 ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ConstrainedEndPoint2¶
-
AestheticFaceBlendBuilder.
ConstrainedEndPoint2
¶ Returns or sets the end point2
-------------------------------------
Getter Method
Signature
ConstrainedEndPoint2
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstrainedEndPoint2
Parameters: endPoint2 ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ConstrainedStartPoint1¶
-
AestheticFaceBlendBuilder.
ConstrainedStartPoint1
¶ Returns or sets the start point1
-------------------------------------
Getter Method
Signature
ConstrainedStartPoint1
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstrainedStartPoint1
Parameters: startPoint1 ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ConstrainedStartPoint2¶
-
AestheticFaceBlendBuilder.
ConstrainedStartPoint2
¶ Returns or sets the start point2
-------------------------------------
Getter Method
Signature
ConstrainedStartPoint2
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstrainedStartPoint2
Parameters: startPoint2 ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Continuity¶
-
AestheticFaceBlendBuilder.
Continuity
¶ Returns the continuity
-------------------------------------
Getter Method
Signature
Continuity
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
Features.AestheticFaceBlendBuilder.Chain1Continuity()
andFeatures.AestheticFaceBlendBuilder.Chain2Continuity()
instead.License requirements: None.
CurvatureTolerance¶
-
AestheticFaceBlendBuilder.
CurvatureTolerance
¶ Returns or sets the curvature tolerance
-------------------------------------
Getter Method
Signature
CurvatureTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurvatureTolerance
Parameters: curvatureTolerance (float) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Degrees¶
-
AestheticFaceBlendBuilder.
Degrees
¶ Returns the degrees
-------------------------------------
Getter Method
Signature
Degrees
Returns: Return type: NXOpen.GeometricUtilities.DegreesAndSegmentsOrPatchesBuilder
New in version NX7.5.0.
License requirements: None.
FaceChain1¶
-
AestheticFaceBlendBuilder.
FaceChain1
¶ Returns the face chain1
-------------------------------------
Getter Method
Signature
FaceChain1
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
FaceChain2¶
-
AestheticFaceBlendBuilder.
FaceChain2
¶ Returns the face chain2
-------------------------------------
Getter Method
Signature
FaceChain2
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
IsAccelerated¶
-
AestheticFaceBlendBuilder.
IsAccelerated
¶ Returns or sets the method to control the shape
-------------------------------------
Getter Method
Signature
IsAccelerated
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsAccelerated
Parameters: isAccelerated (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsBezier¶
-
AestheticFaceBlendBuilder.
IsBezier
¶ Returns or sets the bezier
-------------------------------------
Getter Method
Signature
IsBezier
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsBezier
Parameters: isBezier (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsCenterlineCurve¶
-
AestheticFaceBlendBuilder.
IsCenterlineCurve
¶ Returns or sets the centerline curve
-------------------------------------
Getter Method
Signature
IsCenterlineCurve
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCenterlineCurve
Parameters: isCenterlineCurve (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsMinimumRadius¶
-
AestheticFaceBlendBuilder.
IsMinimumRadius
¶ Returns or sets the is min radius
-------------------------------------
Getter Method
Signature
IsMinimumRadius
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsMinimumRadius
Parameters: isMinimumRadius (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsMinimumSubtendedAngle¶
-
AestheticFaceBlendBuilder.
IsMinimumSubtendedAngle
¶ Returns or sets the minimum subtended angle flag
-------------------------------------
Getter Method
Signature
IsMinimumSubtendedAngle
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsMinimumSubtendedAngle
Parameters: isMinimumSubtendedAngle (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsRationalOutput¶
-
AestheticFaceBlendBuilder.
IsRationalOutput
¶ Returns or sets the rational output
-------------------------------------
Getter Method
Signature
IsRationalOutput
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsRationalOutput
Parameters: isRationalOutput (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsSameTransition¶
-
AestheticFaceBlendBuilder.
IsSameTransition
¶ Returns or sets the blend cross section is using the same transition as blend tangent or not
-------------------------------------
Getter Method
Signature
IsSameTransition
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSameTransition
Parameters: isSameTransition (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsSewAllFaces¶
-
AestheticFaceBlendBuilder.
IsSewAllFaces
¶ Returns or sets the is sew faces
-------------------------------------
Getter Method
Signature
IsSewAllFaces
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSewAllFaces
Parameters: isSewFaces (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsTrimInputFaces¶
-
AestheticFaceBlendBuilder.
IsTrimInputFaces
¶ Returns or sets the is trim faces
-------------------------------------
Getter Method
Signature
IsTrimInputFaces
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsTrimInputFaces
Parameters: isTrimFaces (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsWashout1¶
-
AestheticFaceBlendBuilder.
IsWashout1
¶ Returns or sets the washout1
-------------------------------------
Getter Method
Signature
IsWashout1
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsWashout1
Parameters: isWashout1 (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
IsWashout2¶
-
AestheticFaceBlendBuilder.
IsWashout2
¶ Returns or sets the toggle washout2
-------------------------------------
Getter Method
Signature
IsWashout2
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsWashout2
Parameters: isWashout2 (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
LimitsList¶
-
AestheticFaceBlendBuilder.
LimitsList
¶ Returns the trim object collector list
-------------------------------------
Getter Method
Signature
LimitsList
Returns: Return type: NXOpen.GeometricUtilities.BlendLimitsData
New in version NX8.0.0.
License requirements: None.
MinimumEdgeLength¶
-
AestheticFaceBlendBuilder.
MinimumEdgeLength
¶ Returns or sets the max edge length
-------------------------------------
Getter Method
Signature
MinimumEdgeLength
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumEdgeLength
Parameters: minEdgeLength (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
MinimumRadius¶
-
AestheticFaceBlendBuilder.
MinimumRadius
¶ Returns the min radius
-------------------------------------
Getter Method
Signature
MinimumRadius
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
MinimumSubtendedAngle¶
-
AestheticFaceBlendBuilder.
MinimumSubtendedAngle
¶ Returns or sets the minimum subtended angle
-------------------------------------
Getter Method
Signature
MinimumSubtendedAngle
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumSubtendedAngle
Parameters: minimumSubtendedAngle (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ParameterSpine¶
-
AestheticFaceBlendBuilder.
ParameterSpine
¶ Returns the parameter spine
-------------------------------------
Getter Method
Signature
ParameterSpine
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
PositionTolerance¶
-
AestheticFaceBlendBuilder.
PositionTolerance
¶ Returns or sets the position tolerance
-------------------------------------
Getter Method
Signature
PositionTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositionTolerance
Parameters: positionTolerance (float) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RelativeEndBlendEndPoint¶
-
AestheticFaceBlendBuilder.
RelativeEndBlendEndPoint
¶ Returns or sets the relative end point on the washout curve of end blend.
-------------------------------------
Getter Method
Signature
RelativeEndBlendEndPoint
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelativeEndBlendEndPoint
Parameters: endPoint (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RelativeEndBlendStartPoint¶
-
AestheticFaceBlendBuilder.
RelativeEndBlendStartPoint
¶ Returns or sets the relative start point on the washout curve of end blend.
-------------------------------------
Getter Method
Signature
RelativeEndBlendStartPoint
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelativeEndBlendStartPoint
Parameters: startPoint (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RelativeStartBlendEndPoint¶
-
AestheticFaceBlendBuilder.
RelativeStartBlendEndPoint
¶ Returns or sets the relative end point on the washout curve of start blend.
-------------------------------------
Getter Method
Signature
RelativeStartBlendEndPoint
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelativeStartBlendEndPoint
Parameters: endPoint (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RelativeStartBlendStartPoint¶
-
AestheticFaceBlendBuilder.
RelativeStartBlendStartPoint
¶ Returns or sets the relative start point on the washout curve of start blend.
-------------------------------------
Getter Method
Signature
RelativeStartBlendStartPoint
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelativeStartBlendStartPoint
Parameters: startPoint (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ReverseNormal1¶
-
AestheticFaceBlendBuilder.
ReverseNormal1
¶ Returns or sets the reverse normal1
-------------------------------------
Getter Method
Signature
ReverseNormal1
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseNormal1
Parameters: reverseNormal1 (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ReverseNormal2¶
-
AestheticFaceBlendBuilder.
ReverseNormal2
¶ Returns or sets the reverse normal2
-------------------------------------
Getter Method
Signature
ReverseNormal2
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseNormal2
Parameters: reverseNormal2 (bool) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RhoOption¶
-
AestheticFaceBlendBuilder.
RhoOption
¶ Returns or sets the rho option
-------------------------------------
Getter Method
Signature
RhoOption
Returns: Return type: NXOpen.Features.AestheticFaceBlendBuilderRhoType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RhoOption
Parameters: rhoType ( NXOpen.Features.AestheticFaceBlendBuilderRhoType
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RhoValue¶
-
AestheticFaceBlendBuilder.
RhoValue
¶ Returns or sets the rho value
-------------------------------------
Getter Method
Signature
RhoValue
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RhoValue
Parameters: rhoValue (float) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SectionAlignmentVector¶
-
AestheticFaceBlendBuilder.
SectionAlignmentVector
¶ Returns or sets the section alignment vector
-------------------------------------
Getter Method
Signature
SectionAlignmentVector
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionAlignmentVector
Parameters: sectionAlignmentVector ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SectionScaling1¶
-
AestheticFaceBlendBuilder.
SectionScaling1
¶ Returns the section scaling
-------------------------------------
Getter Method
Signature
SectionScaling1
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SectionScaling2¶
-
AestheticFaceBlendBuilder.
SectionScaling2
¶ Returns the section scaling2
-------------------------------------
Getter Method
Signature
SectionScaling2
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SegmentationOption¶
-
AestheticFaceBlendBuilder.
SegmentationOption
¶ Returns or sets the segmentation option
-------------------------------------
Getter Method
Signature
SegmentationOption
Returns: Return type: NXOpen.Features.AestheticFaceBlendBuilderSegmentationType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SegmentationOption
Parameters: segmentationOption ( NXOpen.Features.AestheticFaceBlendBuilderSegmentationType
) –New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ShapeOption¶
-
AestheticFaceBlendBuilder.
ShapeOption
¶ Returns or sets the shape option
-------------------------------------
Getter Method
Signature
ShapeOption
Returns: Return type: NXOpen.Features.AestheticFaceBlendBuilderShapeType
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
Features.AestheticFaceBlendBuilder.IsAccelerated()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ShapeOption
Parameters: shapeOption ( NXOpen.Features.AestheticFaceBlendBuilderShapeType
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
Features.AestheticFaceBlendBuilder.Accelerated()
instead.License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
TangentMagnitude¶
-
AestheticFaceBlendBuilder.
TangentMagnitude
¶ Returns the tangent magnitude
-------------------------------------
Getter Method
Signature
TangentMagnitude
Returns: Return type: NXOpen.GeometricUtilities.TangentMagnitudeBuilder
New in version NX8.0.0.
License requirements: None.
TangentTolerance¶
-
AestheticFaceBlendBuilder.
TangentTolerance
¶ Returns or sets the tangent tolerance
-------------------------------------
Getter Method
Signature
TangentTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TangentTolerance
Parameters: tangentTolerance (float) – New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
Validate¶
-
AestheticFaceBlendBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.