AestheticFaceBlendBuilderBlendFacesType Enumeration¶
NXOpen.Features.AestheticFaceBlendBuilder.BlendFacesType is an alias for NXOpen.Features.AestheticFaceBlendBuilderBlendFacesType
-
class
NXOpen.Features.
AestheticFaceBlendBuilderBlendFacesType
¶ Bases:
object
Trimming options
Enum Members
Enum Member Enum Member Description TrimtoAllInputFaces Trims all input faces. TrimtoShortInputFaces Trims short input faces. TrimtoLongInputFaces Trims long input faces. DoNotTrimBlendFaces This option controls to trim blend faces or not -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-