BlendLimitsData Class¶
-
class
NXOpen.GeometricUtilities.
BlendLimitsData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.BlendLimitsData
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CapsList | Returns the caps list |
Tag | Returns the Tag for this object. |
UserSelectedObjects | Returns or sets the use plane cap blend |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CapsList¶
-
BlendLimitsData.
CapsList
¶ Returns the caps list
-------------------------------------
Getter Method
Signature
CapsList
Returns: Return type: NXOpen.TaggedObjectList
New in version NX5.0.0.
License requirements: None.
UserSelectedObjects¶
-
BlendLimitsData.
UserSelectedObjects
¶ Returns or sets the use plane cap blend
-------------------------------------
Getter Method
Signature
UserSelectedObjects
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserSelectedObjects
Parameters: useSelectedObject (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
BlendLimitsData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.