TangentMagnitudeBuilder Class¶
-
class
NXOpen.GeometricUtilities.
TangentMagnitudeBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class provides ability to specify the start and end tangent magnitude values.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
EndTangentMagnitude | Returns the end tangent magnitude |
StartTangentMagnitude | Returns the start tangent magnitude |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EndTangentMagnitude¶
-
TangentMagnitudeBuilder.
EndTangentMagnitude
¶ Returns the end tangent magnitude
-------------------------------------
Getter Method
Signature
EndTangentMagnitude
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
StartTangentMagnitude¶
-
TangentMagnitudeBuilder.
StartTangentMagnitude
¶ Returns the start tangent magnitude
-------------------------------------
Getter Method
Signature
StartTangentMagnitude
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TangentMagnitudeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.