Continuity Class¶
-
class
NXOpen.GeometricUtilities.
Continuity
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.Continuity
Allows user to specify continuity constraint surface construction.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ConstraintFaces | Returns the constraint face collector. |
ContinuityType | Returns or sets the continuity type. |
IsFixed | Returns or sets the value indicating if a continuity constraint is of fixed type. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ContinuityContinuityTypes Enumeration | Continuity type. |
Property Detail¶
ConstraintFaces¶
-
Continuity.
ConstraintFaces
¶ Returns the constraint face collector.
-------------------------------------
Getter Method
Signature
ConstraintFaces
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
ContinuityType¶
-
Continuity.
ContinuityType
¶ Returns or sets the continuity type.
If continuity = G0, then constraint face selector is disabled.
-------------------------------------
Getter Method
Signature
ContinuityType
Returns: Return type: NXOpen.GeometricUtilities.ContinuityContinuityTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContinuityType
Parameters: continuityType ( NXOpen.GeometricUtilities.ContinuityContinuityTypes
) –New in version NX5.0.0.
License requirements: None.
IsFixed¶
-
Continuity.
IsFixed
¶ Returns or sets the value indicating if a continuity constraint is of fixed type.
This flag is valid for
NXOpen.GeometricUtilities.ContinuityContinuityTypes.G1
,NXOpen.GeometricUtilities.ContinuityContinuityTypes.G2
,NXOpen.GeometricUtilities.ContinuityContinuityTypes.G3
types only.-------------------------------------
Getter Method
Signature
IsFixed
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsFixed
Parameters: isFixed (bool) – New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
Continuity.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.