AestheticFaceBlendBuilderRhoType Enumeration¶
NXOpen.Features.AestheticFaceBlendBuilder.RhoType is an alias for NXOpen.Features.AestheticFaceBlendBuilderRhoType
-
class
NXOpen.Features.
AestheticFaceBlendBuilderRhoType
¶ Bases:
object
Rho options
Enum Members
Enum Member Enum Member Description Relative Relative Rho: it’s the ratio of BaseRadius/(BaseRadius + CenterRadius) Absolute Absolute Rho: does not take into account the subtended angle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-