AestheticFaceBlendBuilderBlendType Enumeration¶
NXOpen.Features.AestheticFaceBlendBuilder.BlendType is an alias for NXOpen.Features.AestheticFaceBlendBuilderBlendType
-
class
NXOpen.Features.
AestheticFaceBlendBuilderBlendType
¶ Bases:
object
Tangent method will create tangent lines based on the method employed.
Enum Members
Enum Member Enum Member Description Radius Radius of the rolling ball is used to create the tangent lines. ChordLength Chord Length will keep the appearance of a constant width blend through areas which have changing angles between the input walls. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-