AestheticFaceBlendBuilderCenterType Enumeration¶
NXOpen.Features.AestheticFaceBlendBuilder.CenterType is an alias for NXOpen.Features.AestheticFaceBlendBuilderCenterType
-
class
NXOpen.Features.
AestheticFaceBlendBuilderCenterType
¶ Bases:
object
Center methods will define peak of the blend
Enum Members
Enum Member Enum Member Description CenterRadius Center radius option. Rho Rho is the ratio of the center radius and the base radius. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-