ViewStyleBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the View Style Builder (Drawings.
ViewStyleBuilder) which manages all the style attributes related * to the view including base view, projected view, drawing view, detail view, broken view, section view etc. * To obtain an instance of this class, we need to follow the steps: create a new view, click the view style * button, edit the view style attributes.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ProjectedViewOrientation | Returns the projected view orientation builder |
SecondaryComponents | Returns the secondary components style builder of the view style builder which represents the secondary geometry tab on the View Style Dialog |
Tag | Returns the Tag for this object. |
ViewCommonViewLabel | Returns the view common label builder |
ViewProjectedArrowSettings | Returns the projected Arrow Settings builder |
ViewProjectedViewSettings | Returns the projected View Settings builder |
ViewSectionLineStyleBuilder | Returns the view section line builder |
ViewStyleBase | Returns the Base style builder of the view style builder which represents the base tab on the View Style Dialog |
ViewStyleDetail | Returns the Detail style builder of the view style builder which represents the detail tab on the View Style Dialog |
ViewStyleGeneral | Returns the General style builder of the view style builder which represents the general tab on the View Style Dialog |
ViewStyleHiddenLines | Returns the Hidden Lines style builder of the view style builder which represents the hidden lines tab on the View Style Dialog |
ViewStyleInheritPmi | Returns the Inherit PMI style builder of the view style builder which represents the inherit PMI tab on the View Style Dialog |
ViewStyleOrientation | Returns the Orientation style builder of the view style builder which represents the orientation tab on the View Style Dialog |
ViewStylePerspective | Returns the Perspective style builder of the view style builder which represents the perspective tab on the View Style Dialog |
ViewStyleProjected | Returns the projected style builder of the view style builder which represents the projected tab on the View Style Dialog |
ViewStyleSection | Returns the Section style builder of the view style builder which represents the section tab on the View Style Dialog |
ViewStyleSectionConstraints | Returns the Section Constraints style builder of the view style builder which represents the section constraints tab on the View Style Dialog |
ViewStyleShading | Returns the Shading style builder of the view style builder which represents the shading tab on the View Style Dialog |
ViewStyleShipDraftingViewLinesList | Returns the Ship Drafting View lines builder of the view style builder which represents the ship drafting view lines on the View Style Dialog |
ViewStyleSingleLineList | Returns the Ship building lines style builder of the view style builder which represents the ship building lines tab on the View Style Dialog |
ViewStyleSmoothEdges | Returns the Smooth Edges style builder of the view style builder which represents the smooth edges tab on the View Style Dialog |
ViewStyleThreads | Returns the Threads style builder of the view style builder which represents the threads tab on the View Style Dialog |
ViewStyleTraceLines | Returns the Trace lines style builder of the view style builder which represents the trace lines tab on the View Style Dialog |
ViewStyleVirtualIntersections | Returns the Virtual intersections style builder of the view style builder which represents the virtual intersections tab on the View Style Dialog |
ViewStyleVisibleLines | Returns the Visible lines style builder of the view style builder which represents the visible lines tab on the View Style Dialog |
Methods¶
Method | Description |
---|---|
FindShipDraftingViewLinesBuilderByName | Gets the NXOpen.Drawings.ShipDraftingViewLinesBuilder with the given FeatureName and FeatureSubName |
GetAllViewStyleFPCallouts | Retrieves all the Callouts on the Flat Pattern Tab on the View Style Dialog |
GetAllViewStyleFPCurves | Retrieves all the Curves on the Flat Pattern Tab on the View Style Dialog |
GetViewStyleFPCallout | Retrieves a specified Callout on the Flat Pattern Tab on the View Style Dialog |
GetViewStyleFPCalloutConfig | Retrieves the callout configuration on the Flat Pattern Tab on the View Style Dialog |
GetViewStyleFPCurve | Retrieves a specified Curve on the Flat Pattern Tab on the View Style Dialog |
InheritSettingsFromCustomerDefault | Inherit Settings From Customer Default |
InheritSettingsFromPreferences | Inherit Settings From Preference |
InheritSettingsFromSelectedObjects | Inherit Settings From Selected Objects |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ProjectedViewOrientation¶
-
ViewStyleBuilder.
ProjectedViewOrientation
¶ Returns the projected view orientation builder
-------------------------------------
Getter Method
Signature
ProjectedViewOrientation
Returns: Return type: NXOpen.Drawings.ProjectedViewOrientationBuilder
New in version NX9.0.0.
License requirements: None.
SecondaryComponents¶
-
ViewStyleBuilder.
SecondaryComponents
¶ Returns the secondary components style builder of the view style builder which represents the secondary geometry tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
SecondaryComponents
Returns: Returns the Secondary Components sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleSecondaryComponentsBuilder
New in version NX11.0.0.
License requirements: drafting (“DRAFTING”)
ViewCommonViewLabel¶
-
ViewStyleBuilder.
ViewCommonViewLabel
¶ Returns the view common label builder
-------------------------------------
Getter Method
Signature
ViewCommonViewLabel
Returns: Return type: NXOpen.Drawings.ViewCommonViewLabelBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
ViewProjectedArrowSettings¶
-
ViewStyleBuilder.
ViewProjectedArrowSettings
¶ Returns the projected Arrow Settings builder
-------------------------------------
Getter Method
Signature
ViewProjectedArrowSettings
Returns: Return type: NXOpen.Drawings.ViewProjectedArrowSettingsBuilder
New in version NX9.0.0.
License requirements: None.
ViewProjectedViewSettings¶
-
ViewStyleBuilder.
ViewProjectedViewSettings
¶ Returns the projected View Settings builder
-------------------------------------
Getter Method
Signature
ViewProjectedViewSettings
Returns: Return type: NXOpen.Drawings.ViewProjectedViewSettingsBuilder
New in version NX9.0.0.
License requirements: None.
ViewSectionLineStyleBuilder¶
-
ViewStyleBuilder.
ViewSectionLineStyleBuilder
¶ Returns the view section line builder
-------------------------------------
Getter Method
Signature
ViewSectionLineStyleBuilder
Returns: Return type: NXOpen.Drawings.ViewSectionLineBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleBase¶
-
ViewStyleBuilder.
ViewStyleBase
¶ Returns the Base style builder of the view style builder which represents the base tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleBase
Returns: Returns the Base sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleBaseBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleDetail¶
-
ViewStyleBuilder.
ViewStyleDetail
¶ Returns the Detail style builder of the view style builder which represents the detail tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleDetail
Returns: Returns the Detail sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleDetailBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleGeneral¶
-
ViewStyleBuilder.
ViewStyleGeneral
¶ Returns the General style builder of the view style builder which represents the general tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleGeneral
Returns: Returns the General sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleGeneralBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleInheritPmi¶
-
ViewStyleBuilder.
ViewStyleInheritPmi
¶ Returns the Inherit PMI style builder of the view style builder which represents the inherit PMI tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleInheritPmi
Returns: Returns the Inherit Pmi sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleInheritPmiBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleOrientation¶
-
ViewStyleBuilder.
ViewStyleOrientation
¶ Returns the Orientation style builder of the view style builder which represents the orientation tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleOrientation
Returns: Returns the Orientation sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleOrientationBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStylePerspective¶
-
ViewStyleBuilder.
ViewStylePerspective
¶ Returns the Perspective style builder of the view style builder which represents the perspective tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStylePerspective
Returns: Returns the Perspective sub-builder on View Style Return type: NXOpen.Drawings.ViewStylePerspectiveBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleProjected¶
-
ViewStyleBuilder.
ViewStyleProjected
¶ Returns the projected style builder of the view style builder which represents the projected tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleProjected
Returns: Returns the Projected sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleProjectedBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleSection¶
-
ViewStyleBuilder.
ViewStyleSection
¶ Returns the Section style builder of the view style builder which represents the section tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleSection
Returns: Returns the Section sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleSectionBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleSectionConstraints¶
-
ViewStyleBuilder.
ViewStyleSectionConstraints
¶ Returns the Section Constraints style builder of the view style builder which represents the section constraints tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleSectionConstraints
Returns: Returns the Section Constraints sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleSectionConstraintsBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleShading¶
-
ViewStyleBuilder.
ViewStyleShading
¶ Returns the Shading style builder of the view style builder which represents the shading tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleShading
Returns: Returns the Shading sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleShadingBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleShipDraftingViewLinesList¶
-
ViewStyleBuilder.
ViewStyleShipDraftingViewLinesList
¶ Returns the Ship Drafting View lines builder of the view style builder which represents the ship drafting view lines on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleShipDraftingViewLinesList
Returns: Returns the Ship Drafting View Lines sub-builders on View Style Return type: NXOpen.Drawings.ShipDraftingViewLinesBuilderList
New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
ViewStyleSingleLineList¶
-
ViewStyleBuilder.
ViewStyleSingleLineList
¶ Returns the Ship building lines style builder of the view style builder which represents the ship building lines tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleSingleLineList
Returns: Returns the Shipbuilding Lines sub-builders on View Style Return type: NXOpen.Drawings.ViewStyleShipbuildingLinesBuilderList
New in version NX8.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleSmoothEdges¶
-
ViewStyleBuilder.
ViewStyleSmoothEdges
¶ Returns the Smooth Edges style builder of the view style builder which represents the smooth edges tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleSmoothEdges
Returns: Returns the Smooth Edges sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleSmoothEdgesBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleThreads¶
-
ViewStyleBuilder.
ViewStyleThreads
¶ Returns the Threads style builder of the view style builder which represents the threads tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleThreads
Returns: Returns the Threads sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleThreadsBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleTraceLines¶
-
ViewStyleBuilder.
ViewStyleTraceLines
¶ Returns the Trace lines style builder of the view style builder which represents the trace lines tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleTraceLines
Returns: Returns the Trace Lines sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleTraceLinesBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleVirtualIntersections¶
-
ViewStyleBuilder.
ViewStyleVirtualIntersections
¶ Returns the Virtual intersections style builder of the view style builder which represents the virtual intersections tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleVirtualIntersections
Returns: Returns the Intersections sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleVirtualIntersectionsBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewStyleVisibleLines¶
-
ViewStyleBuilder.
ViewStyleVisibleLines
¶ Returns the Visible lines style builder of the view style builder which represents the visible lines tab on the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewStyleVisibleLines
Returns: Returns the Visible Lines sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleVisibleLinesBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
FindShipDraftingViewLinesBuilderByName¶
-
ViewStyleBuilder.
FindShipDraftingViewLinesBuilderByName
¶ Gets the
NXOpen.Drawings.ShipDraftingViewLinesBuilder
with the given FeatureName and FeatureSubNameSignature
FindShipDraftingViewLinesBuilderByName(featureName, featureSubName)
Parameters: - featureName (str) –
- featureSubName (str) –
Returns: Returns the Ship Drafting View Lines sub-builders with the given FeatureName and FeatureSubName
Return type: New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
GetAllViewStyleFPCallouts¶
-
ViewStyleBuilder.
GetAllViewStyleFPCallouts
¶ Retrieves all the Callouts on the Flat Pattern Tab on the View Style Dialog
Signature
GetAllViewStyleFPCallouts()
Returns: Returns all the Flat Pattern Callout sub-builders on View Style Return type: list of NXOpen.Drawings.ViewStyleFPCalloutsBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
GetAllViewStyleFPCurves¶
-
ViewStyleBuilder.
GetAllViewStyleFPCurves
¶ Retrieves all the Curves on the Flat Pattern Tab on the View Style Dialog
Signature
GetAllViewStyleFPCurves()
Returns: Returns all the Flat Pattern Curve sub-builders on View Style Return type: list of NXOpen.Drawings.ViewStyleFPCurvesBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
GetViewStyleFPCallout¶
-
ViewStyleBuilder.
GetViewStyleFPCallout
¶ Retrieves a specified Callout on the Flat Pattern Tab on the View Style Dialog
Signature
GetViewStyleFPCallout(type)
Parameters: type (str) – Indicates which flat pattern callout Returns: Returns the particular Flat Pattern Callout sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleFPCalloutsBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
GetViewStyleFPCalloutConfig¶
-
ViewStyleBuilder.
GetViewStyleFPCalloutConfig
¶ Retrieves the callout configuration on the Flat Pattern Tab on the View Style Dialog
Signature
GetViewStyleFPCalloutConfig()
Returns: Returns the Flat Pattern Callout Config sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleFPCalloutConfigBuilder
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
GetViewStyleFPCurve¶
-
ViewStyleBuilder.
GetViewStyleFPCurve
¶ Retrieves a specified Curve on the Flat Pattern Tab on the View Style Dialog
Signature
GetViewStyleFPCurve(type)
Parameters: type ( NXOpen.SheetMetal.FlatPatternSettingsFlatPatternObjectType
) – Indicates which flat pattern curveReturns: Returns the particular Flat Pattern Curve sub-builder on View Style Return type: NXOpen.Drawings.ViewStyleFPCurvesBuilder
New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromCustomerDefault¶
-
ViewStyleBuilder.
InheritSettingsFromCustomerDefault
¶ Inherit Settings From Customer Default
Signature
InheritSettingsFromCustomerDefault()
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromPreferences¶
-
ViewStyleBuilder.
InheritSettingsFromPreferences
¶ Inherit Settings From Preference
Signature
InheritSettingsFromPreferences()
New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
InheritSettingsFromSelectedObjects¶
-
ViewStyleBuilder.
InheritSettingsFromSelectedObjects
¶ Inherit Settings From Selected Objects
Signature
InheritSettingsFromSelectedObjects(selectedObject)
Parameters: selectedObject ( NXOpen.NXObject
) – The selected annotation or table or view instance object. None is not allowed.New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
ViewStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.