ViewStylePerspectiveBuilder Class¶
-
class
NXOpen.Drawings.
ViewStylePerspectiveBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the PERSPECTIVE tab on the View Style Dialog (Drawings.
ViewStylePerspectiveBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
BackClip | Returns or sets the back clip toggle on the PERSPECTIVE tab of the View Style Dialog |
BackClipDistance | Returns or sets the back clip distance data on the PERSPECTIVE tab of the View Style Dialog |
FrontClip | Returns or sets the front clip toggle on the PERSPECTIVE tab of the View Style Dialog |
FrontClipDistance | Returns or sets the front clip distance data on the PERSPECTIVE tab of the View Style Dialog |
Perspective | Returns or sets the perspective toggle on the PERSPECTIVE tab of the View Style Dialog |
PerspectiveDistance | Returns or sets the perspective distance data on the PERSPECTIVE tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
ViewOrigin | Returns or sets the perspective view origin on the PERSPECTIVE tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BackClip¶
-
ViewStylePerspectiveBuilder.
BackClip
¶ Returns or sets the back clip toggle on the PERSPECTIVE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
BackClip
Returns: Returns the back clip toggle value that is on the perspective sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BackClip
Parameters: backClipToggle (bool) – Sets a new back clip toggle value on the perspective sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
BackClipDistance¶
-
ViewStylePerspectiveBuilder.
BackClipDistance
¶ Returns or sets the back clip distance data on the PERSPECTIVE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
BackClipDistance
Returns: Returns the back clip distance that is on the perspective sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BackClipDistance
Parameters: backClipDistanceData (float) – Sets a new back clip distance on the perspective sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
FrontClip¶
-
ViewStylePerspectiveBuilder.
FrontClip
¶ Returns or sets the front clip toggle on the PERSPECTIVE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
FrontClip
Returns: Returns the front clip toggle value that is on the perspective sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontClip
Parameters: frontClipToggle (bool) – Sets a new front clip toggle value on the perspective sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
FrontClipDistance¶
-
ViewStylePerspectiveBuilder.
FrontClipDistance
¶ Returns or sets the front clip distance data on the PERSPECTIVE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
FrontClipDistance
Returns: Returns the front clip distance that is on the perspective sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrontClipDistance
Parameters: frontClipDistanceData (float) – Sets a new front clip distance on the perspective sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Perspective¶
-
ViewStylePerspectiveBuilder.
Perspective
¶ Returns or sets the perspective toggle on the PERSPECTIVE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Perspective
Returns: Returns the perspective toggle value that is on the perspective sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Perspective
Parameters: perspectiveToggle (bool) – Sets a new perspective toggle value on the perspective sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
PerspectiveDistance¶
-
ViewStylePerspectiveBuilder.
PerspectiveDistance
¶ Returns or sets the perspective distance data on the PERSPECTIVE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
PerspectiveDistance
Returns: Returns the perspective distance that is on the perspective sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PerspectiveDistance
Parameters: perspectiveDistanceData (float) – Sets a new perspective distance on the perspective sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ViewOrigin¶
-
ViewStylePerspectiveBuilder.
ViewOrigin
¶ Returns or sets the perspective view origin on the PERSPECTIVE tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ViewOrigin
Returns: Returns the view origin that is on the perspective sub-builder Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ViewOrigin
Parameters: viewOrigin ( NXOpen.Point3d
) – Sets a new view origin on the perspective sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStylePerspectiveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.