ShipDraftingViewLinesBuilder Class¶
-
class
NXOpen.Drawings.
ShipDraftingViewLinesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a ship view lines block
To create a new instance of this class, use
NXOpen.Drawings.DraftingViewCollection.CreateShipDraftingViewLinesBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
NonSectionedHiddenColor | Returns or sets the non-sectioned hidden color on the Ship Structure Lines |
NonSectionedHiddenFont | Returns or sets the non-sectioned hidden font on the Ship Structure Lines |
NonSectionedHiddenWidth | Returns or sets the non-sectioned hidden width on the Ship Structure Lines |
NonSectionedSecondaryHiddenColor | Returns or sets the Secondary non-sectioned hidden color on the Ship Structure Lines |
NonSectionedSecondaryHiddenFont | Returns or sets the Secondary non-sectioned hidden font on the Ship Structure Lines |
NonSectionedSecondaryHiddenWidth | Returns or sets the Secondary non-sectioned hidden width on the Ship Structure Lines |
NonSectionedSecondaryVisibleColor | Returns or sets the Secondary non-sectioned visible color on the Ship Structure Lines |
NonSectionedSecondaryVisibleFont | Returns or sets the Secondary non-sectioned visible font on the Ship Structure Lines |
NonSectionedSecondaryVisibleWidth | Returns or sets the Secondary non-sectioned visible width on the Ship Structure Lines |
NonSectionedVisibleColor | Returns or sets the non-sectioned visible color on the Ship Structure Lines |
NonSectionedVisibleFont | Returns or sets the non-sectioned visible font on the Ship Structure Lines |
NonSectionedVisibleWidth | Returns or sets the non-sectioned visible width on the Ship Structure Lines |
SectionedHiddenColor | Returns or sets the sectioned hidden color on the Ship Structure Lines |
SectionedHiddenFont | Returns or sets the sectioned hidden font on the Ship Structure Lines |
SectionedHiddenWidth | Returns or sets the sectioned hidden width on the Ship Structure Lines |
SectionedSecondaryHiddenColor | Returns or sets the Secondary sectioned hidden color on the Ship Structure Lines |
SectionedSecondaryHiddenFont | Returns or sets the Secondary sectioned hidden font on the Ship Structure Lines |
SectionedSecondaryHiddenWidth | Returns or sets the Secondary sectioned hidden width on the Ship Structure Lines |
SectionedSecondaryVisibleColor | Returns or sets the Secondary sectioned visible color on the Ship Structure Lines |
SectionedSecondaryVisibleFont | Returns or sets the Secondary sectioned visible font on the Ship Structure Lines |
SectionedSecondaryVisibleWidth | Returns or sets the Secondary sectioned visible width on the Ship Structure Lines |
SectionedVisibleColor | Returns or sets the sectioned visible color on the Ship Structure Lines |
SectionedVisibleFont | Returns or sets the sectioned visible font on the Ship Structure Lines |
SectionedVisibleWidth | Returns or sets the sectioned visible width on the Ship Structure Lines |
SingleLineRepresentation | Returns or sets the single line representation toggle |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NonSectionedSecondaryVisibleColor¶
-
ShipDraftingViewLinesBuilder.
NonSectionedSecondaryVisibleColor
¶ Returns or sets the Secondary non-sectioned visible color on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedSecondaryVisibleColor
Returns: Returns the non-sectioned visible color that is on the ship drafting view lines sub-builder Return type: Id New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedSecondaryVisibleColor
Parameters: nonSectionedSecondaryVisibleColor (Id) – Sets a new non-sectined visible color on the ship drafting view lines sub-builder New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
NonSectionedSecondaryVisibleFont¶
-
ShipDraftingViewLinesBuilder.
NonSectionedSecondaryVisibleFont
¶ Returns or sets the Secondary non-sectioned visible font on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedSecondaryVisibleFont
Returns: Returns the non-sectioneed visible font that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Font
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedSecondaryVisibleFont
Parameters: nonSectionedSecondaryVisibleFont ( NXOpen.Preferences.Font
) – Sets a new non-sectioned visible font on the ship drafting view lines sub-builderNew in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
NonSectionedSecondaryVisibleWidth¶
-
ShipDraftingViewLinesBuilder.
NonSectionedSecondaryVisibleWidth
¶ Returns or sets the Secondary non-sectioned visible width on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedSecondaryVisibleWidth
Returns: Returns the non-sectioned visible width that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Width
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedSecondaryVisibleWidth
Parameters: nonSectionedSecondaryVisibleWidth ( NXOpen.Preferences.Width
) – Sets a new non-sectioned visible width on the ship drafting view lines sub-builderNew in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
NonSectionedVisibleColor¶
-
ShipDraftingViewLinesBuilder.
NonSectionedVisibleColor
¶ Returns or sets the non-sectioned visible color on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedVisibleColor
Returns: Returns the non-sectioned visible color that is on the ship drafting view lines sub-builder Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedVisibleColor
Parameters: nonSectionedVisibleColor (Id) – Sets a new non-sectined visible color on the ship drafting view lines sub-builder New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
NonSectionedVisibleFont¶
-
ShipDraftingViewLinesBuilder.
NonSectionedVisibleFont
¶ Returns or sets the non-sectioned visible font on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedVisibleFont
Returns: Returns the non-sectioneed visible font that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Font
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedVisibleFont
Parameters: nonSectionedVisibleFont ( NXOpen.Preferences.Font
) – Sets a new non-sectioned visible font on the ship drafting view lines sub-builderNew in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
NonSectionedVisibleWidth¶
-
ShipDraftingViewLinesBuilder.
NonSectionedVisibleWidth
¶ Returns or sets the non-sectioned visible width on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
NonSectionedVisibleWidth
Returns: Returns the non-sectioned visible width that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Width
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonSectionedVisibleWidth
Parameters: nonSectionedVisibleWidth ( NXOpen.Preferences.Width
) – Sets a new non-sectioned visible width on the ship drafting view lines sub-builderNew in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedSecondaryVisibleColor¶
-
ShipDraftingViewLinesBuilder.
SectionedSecondaryVisibleColor
¶ Returns or sets the Secondary sectioned visible color on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedSecondaryVisibleColor
Returns: Returns the sectioned visible color that is on the ship drafting view lines sub-builder Return type: Id New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedSecondaryVisibleColor
Parameters: sectionedSecondaryVisibleColor (Id) – Sets a new sectined visible color on the ship drafting view lines sub-builder New in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedSecondaryVisibleFont¶
-
ShipDraftingViewLinesBuilder.
SectionedSecondaryVisibleFont
¶ Returns or sets the Secondary sectioned visible font on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedSecondaryVisibleFont
Returns: Returns the sectioneed visible font that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Font
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedSecondaryVisibleFont
Parameters: sectionedSecondaryVisibleFont ( NXOpen.Preferences.Font
) – Sets a new sectioned visible font on the ship drafting view lines sub-builderNew in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedSecondaryVisibleWidth¶
-
ShipDraftingViewLinesBuilder.
SectionedSecondaryVisibleWidth
¶ Returns or sets the Secondary sectioned visible width on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedSecondaryVisibleWidth
Returns: Returns the sectioned visible width that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Width
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedSecondaryVisibleWidth
Parameters: sectionedSecondaryVisibleWidth ( NXOpen.Preferences.Width
) – Sets a new sectioned visible width on the ship drafting view lines sub-builderNew in version NX11.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedVisibleColor¶
-
ShipDraftingViewLinesBuilder.
SectionedVisibleColor
¶ Returns or sets the sectioned visible color on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedVisibleColor
Returns: Returns the sectioned visible color that is on the ship drafting view lines sub-builder Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedVisibleColor
Parameters: sectionedVisibleColor (Id) – Sets a new sectined visible color on the ship drafting view lines sub-builder New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedVisibleFont¶
-
ShipDraftingViewLinesBuilder.
SectionedVisibleFont
¶ Returns or sets the sectioned visible font on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedVisibleFont
Returns: Returns the sectioneed visible font that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Font
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedVisibleFont
Parameters: sectionedVisibleFont ( NXOpen.Preferences.Font
) – Sets a new sectioned visible font on the ship drafting view lines sub-builderNew in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SectionedVisibleWidth¶
-
ShipDraftingViewLinesBuilder.
SectionedVisibleWidth
¶ Returns or sets the sectioned visible width on the Ship Structure Lines
-------------------------------------
Getter Method
Signature
SectionedVisibleWidth
Returns: Returns the sectioned visible width that is the ship drafting view lines sub-builder Return type: NXOpen.Preferences.Width
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionedVisibleWidth
Parameters: sectionedVisibleWidth ( NXOpen.Preferences.Width
) – Sets a new sectioned visible width on the ship drafting view lines sub-builderNew in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
SingleLineRepresentation¶
-
ShipDraftingViewLinesBuilder.
SingleLineRepresentation
¶ Returns or sets the single line representation toggle
-------------------------------------
Getter Method
Signature
SingleLineRepresentation
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SingleLineRepresentation
Parameters: singleLineRepresentation (bool) – New in version NX10.0.0.
License requirements: nx_ship_drafting (“Ship Drafting”)
Method Detail¶
Validate¶
-
ShipDraftingViewLinesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.