ViewStyleProjectedBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleProjectedBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the PROJECTED tab on the View Style Dialog (Drawings.
ViewStyleProjectedBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Align | Returns or sets the projected view style align toggle on the PROJECTED tab of the View Style Dialog |
Gdt | Returns or sets the projected view style gdt toggle on the PROJECTED tab of the View Style Dialog |
Offset | Returns or sets the projected view style offset toggle on the PROJECTED tab of the View Style Dialog |
Orient | Returns or sets the projected view style orient toggle on the PROJECTED tab of the View Style Dialog |
Scale | Returns or sets the projected view style scale toggle on the PROJECTED tab of the View Style Dialog |
Sheet | Returns or sets the projected view style sheet toggle on the PROJECTED tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Align¶
-
ViewStyleProjectedBuilder.
Align
¶ Returns or sets the projected view style align toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Align
Returns: Returns the align toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Align
Parameters: alignToggle (bool) – Sets a new align toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Gdt¶
-
ViewStyleProjectedBuilder.
Gdt
¶ Returns or sets the projected view style gdt toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Gdt
Returns: Returns the gdt toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Gdt
Parameters: gdtToggle (bool) – Sets a new gdt toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Offset¶
-
ViewStyleProjectedBuilder.
Offset
¶ Returns or sets the projected view style offset toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Offset
Returns: Returns the offset toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset
Parameters: offsetToggle (bool) – Sets a new offset toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Orient¶
-
ViewStyleProjectedBuilder.
Orient
¶ Returns or sets the projected view style orient toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Orient
Returns: Returns the orient toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Orient
Parameters: orientToggle (bool) – Sets a new orient toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Scale¶
-
ViewStyleProjectedBuilder.
Scale
¶ Returns or sets the projected view style scale toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Scale
Returns: Returns the scale toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale
Parameters: scaleToggle (bool) – Sets a new scale toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Sheet¶
-
ViewStyleProjectedBuilder.
Sheet
¶ Returns or sets the projected view style sheet toggle on the PROJECTED tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Sheet
Returns: Returns the sheet toggle value that is on the projected sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sheet
Parameters: sheetToggle (bool) – Sets a new sheet toggle value on the projected sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleProjectedBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.