ViewStyleThreadsBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleThreadsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the THREADS tab on the View Style Dialog (Drawings.
ViewStyleThreadsBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
MinimumPitchFieldData | Returns or sets the minimum pitch field on the THREADS tab of the View Style Dialog |
OverrideVisibleThreadColor | Returns or sets the override thread color on the THREADS tab of the View Style Dialog |
StandardData | Returns or sets the standard option data on the THREADS tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
TrueHiddenLine | Returns or sets the true hidden line toggle on the THREADS tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
MinimumPitchFieldData¶
-
ViewStyleThreadsBuilder.
MinimumPitchFieldData
¶ Returns or sets the minimum pitch field on the THREADS tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
MinimumPitchFieldData
Returns: Returns the minimum pitch field data that is on the threads sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumPitchFieldData
Parameters: minimumPitchFieldData (float) – Sets a new minimum pitch field data on the threads sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
OverrideVisibleThreadColor¶
-
ViewStyleThreadsBuilder.
OverrideVisibleThreadColor
¶ Returns or sets the override thread color on the THREADS tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
OverrideVisibleThreadColor
Returns: Returns the override visible color that is on the threads sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverrideVisibleThreadColor
Parameters: overrideVisibleThreadColor (Id) – Sets a new override visible color on the threads sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
StandardData¶
-
ViewStyleThreadsBuilder.
StandardData
¶ Returns or sets the standard option data on the THREADS tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
StandardData
Returns: Returns the standard option that is on the threads sub-builder Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandardData
Parameters: standardOptionData (int) – Sets a new standard option on the threads sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleThreadsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.