ViewStyleSectionBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleSectionBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the SECTION tab on the View Style Dialog (Drawings.
ViewStyleSectionBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AdjacencyToleranceData | Returns or sets the adjacency tolerance on the SECTION tab of the View Style Dialog |
AssemblyTolerance | Returns or sets the assembly tolerance toggle on the SECTION tab of the View Style Dialog |
Background | Returns or sets the background toggle on the SECTION tab of the View Style Dialog |
Bendlines | Returns or sets the bendlines toggle on the SECTION tab of the View Style Dialog |
Crosshatch | Returns or sets the crosshatch toggle on the SECTION tab of the View Style Dialog |
DisplaySectionLine | Returns or sets the display section line toggle on the SECTION tab of the View Style Dialog |
Foreground | Returns or sets the foreground toggle on the SECTION tab of the View Style Dialog |
HiddenLineHatching | Returns or sets the hidden line hatching toggle on the SECTION tab of the View Style Dialog |
RestrictCrosshatchAngle | Returns or sets the restrict crosshatch angle toggle on the SECTION tab of the View Style Dialog |
SheetBodies | Returns or sets the sheet bodies toggle on the SECTION tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdjacencyToleranceData¶
-
ViewStyleSectionBuilder.
AdjacencyToleranceData
¶ Returns or sets the adjacency tolerance on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
AdjacencyToleranceData
Returns: Returns the assembly tolerance that is on the section sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjacencyToleranceData
Parameters: adjacencyToleranceData (float) – Sets a new assembly tolerance on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
AssemblyTolerance¶
-
ViewStyleSectionBuilder.
AssemblyTolerance
¶ Returns or sets the assembly tolerance toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
AssemblyTolerance
Returns: Returns the assembly tolerance toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssemblyTolerance
Parameters: assemblyToleranceToggle (bool) – Sets a new assembly tolerance toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Background¶
-
ViewStyleSectionBuilder.
Background
¶ Returns or sets the background toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Background
Returns: Returns the background toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Background
Parameters: backgroundToggle (bool) – Sets a new background toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Bendlines¶
-
ViewStyleSectionBuilder.
Bendlines
¶ Returns or sets the bendlines toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Bendlines
Returns: Returns the bendlines toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Bendlines
Parameters: bendlinesToggle (bool) – Sets a new bendlines toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Crosshatch¶
-
ViewStyleSectionBuilder.
Crosshatch
¶ Returns or sets the crosshatch toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Crosshatch
Returns: Returns the crosshatch toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Crosshatch
Parameters: crosshatchToggle (bool) – Sets a new crosshatch toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
DisplaySectionLine¶
-
ViewStyleSectionBuilder.
DisplaySectionLine
¶ Returns or sets the display section line toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
DisplaySectionLine
Returns: Returns the display section line toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplaySectionLine
Parameters: displaySectionLine (bool) – Sets a new display section line toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Foreground¶
-
ViewStyleSectionBuilder.
Foreground
¶ Returns or sets the foreground toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Foreground
Returns: Returns the foreground toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Foreground
Parameters: foregroundToggle (bool) – Sets a new foreground toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
RestrictCrosshatchAngle¶
-
ViewStyleSectionBuilder.
RestrictCrosshatchAngle
¶ Returns or sets the restrict crosshatch angle toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
RestrictCrosshatchAngle
Returns: Returns the restrict crosshatch angle toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RestrictCrosshatchAngle
Parameters: restrictCrosshatchAngleToggle (bool) – Sets a new restrict crosshatch angle toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
SheetBodies¶
-
ViewStyleSectionBuilder.
SheetBodies
¶ Returns or sets the sheet bodies toggle on the SECTION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
SheetBodies
Returns: Returns the sheet bodies toggle value that is on the section sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SheetBodies
Parameters: sheetBodiesToggle (bool) – Sets a new sheet bodies toggle value on the section sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.