ViewStyleSmoothEdgesBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleSmoothEdgesBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the SMOOTH EDGES tab on the View Style Dialog (Drawings.
ViewStyleSmoothEdgesBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color on the SMOOTH EDGES tab of the View Style Dialog |
EndGaps | Returns or sets the end gaps toggle on the SMOOTH EDGES tab of the View Style Dialog |
EndGapsDistance | Returns or sets the end gaps data on the SMOOTH EDGES tab of the View Style Dialog |
Font | Returns or sets the font on the SMOOTH EDGES tab of the View Style Dialog |
SmoothEdge | Returns or sets the smooth edge toggle on the SMOOTH EDGES tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the angle tolerance toggle on the SMOOTH EDGES tab of the View Style Dialog |
ToleranceValue | Returns or sets the angle tolerance data on the SMOOTH EDGES tab of the View Style Dialog |
Width | Returns or sets the width on the SMOOTH EDGES tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Color¶
-
ViewStyleSmoothEdgesBuilder.
Color
¶ Returns or sets the color on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Color
Returns: Returns the color that is on the smooth edges sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Color
Parameters: color (Id) – Sets a new color on the smooth edge sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
EndGaps¶
-
ViewStyleSmoothEdgesBuilder.
EndGaps
¶ Returns or sets the end gaps toggle on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
EndGaps
Returns: Returns the end gaps toggle value that is on the smooth edges sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndGaps
Parameters: endGapsToggle (bool) – Sets a new end gaps toggle value on the smooth edge sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
EndGapsDistance¶
-
ViewStyleSmoothEdgesBuilder.
EndGapsDistance
¶ Returns or sets the end gaps data on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
EndGapsDistance
Returns: Returns the end gaps data that is on the smooth edges sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndGapsDistance
Parameters: endGapsData (float) – Sets new end gaps data on the smooth edge sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Font¶
-
ViewStyleSmoothEdgesBuilder.
Font
¶ Returns or sets the font on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Font
Returns: Returns the font that is on the smooth edges sub-builder Return type: NXOpen.Preferences.Font
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Font
Parameters: font ( NXOpen.Preferences.Font
) – Sets a new font on the smooth edge sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
SmoothEdge¶
-
ViewStyleSmoothEdgesBuilder.
SmoothEdge
¶ Returns or sets the smooth edge toggle on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
SmoothEdge
Returns: Returns the smooth edge toggle value that is on the smooth edges sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SmoothEdge
Parameters: smoothEdgesToggle (bool) – Sets a new smooth edge toggle value on the smooth edge sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Tolerance¶
-
ViewStyleSmoothEdgesBuilder.
Tolerance
¶ Returns or sets the angle tolerance toggle on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Returns the tolerance toggle value that is on the smooth edges sub-builder Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: toleranceToggle (bool) – Sets a new tolerance toggle value on the smooth edge sub-builder New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
ToleranceValue¶
-
ViewStyleSmoothEdgesBuilder.
ToleranceValue
¶ Returns or sets the angle tolerance data on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ToleranceValue
Returns: Returns the tolerance data that is on the smooth edges sub-builder Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToleranceValue
Parameters: toleranceData (float) – Sets new tolerance data on the smooth edge sub-builder New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Width¶
-
ViewStyleSmoothEdgesBuilder.
Width
¶ Returns or sets the width on the SMOOTH EDGES tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Width
Returns: Returns the width that is on the smooth edges sub-builder Return type: NXOpen.Preferences.Width
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width
Parameters: width ( NXOpen.Preferences.Width
) – Sets a new width on the smooth edge sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleSmoothEdgesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.