ViewStyleShadingBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleShadingBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the SHADING tab on the View Style Dialog (Drawings.
ViewStyleShadingBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance data on the SHADING tab of the View Style Dialog |
CutFaceColor | Returns or sets the cut face color on the SHADING tab of the View Style Dialog |
EdgeTolerance | Returns or sets the edge tolerance data on the SHADING tab of the View Style Dialog |
FaceTolerance | Returns or sets the face tolerance data on the SHADING tab of the View Style Dialog |
HiddenWireframeColor | Returns or sets the hidden wireframe color on the SHADING tab of the View Style Dialog |
RenderingStyle | Returns or sets the rendering style option on the SHADING tab of the View Style Dialog |
ShadeTolerance | Returns or sets the shade tolerance option on the SHADING tab of the View Style Dialog |
ShininessScale | Returns or sets the shininess scale data on the SHADING tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
TwoSidedLight | Returns or sets the two sided light toggle on the SHADING tab of the View Style Dialog |
VisibleWireframeColor | Returns or sets the visible wireframe color on the SHADING tab of the View Style Dialog |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
ViewStyleShadingBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance data on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Returns the angle tolerance that is on the shading sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleToleranceData (float) – Sets a new angle tolerance on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
CutFaceColor¶
-
ViewStyleShadingBuilder.
CutFaceColor
¶ Returns or sets the cut face color on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
CutFaceColor
Returns: Returns the cut face color that is on the shading sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutFaceColor
Parameters: cutFaceColor (Id) – Sets a new cut face color on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
EdgeTolerance¶
-
ViewStyleShadingBuilder.
EdgeTolerance
¶ Returns or sets the edge tolerance data on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
EdgeTolerance
Returns: Returns the edge tolerance that is on the shading sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeTolerance
Parameters: edgeToleranceData (float) – Sets a new edge tolerance on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
FaceTolerance¶
-
ViewStyleShadingBuilder.
FaceTolerance
¶ Returns or sets the face tolerance data on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
FaceTolerance
Returns: Returns the face tolerance that is on the shading sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceTolerance
Parameters: faceToleranceData (float) – Sets a new face tolerance on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
RenderingStyle¶
-
ViewStyleShadingBuilder.
RenderingStyle
¶ Returns or sets the rendering style option on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
RenderingStyle
Returns: Returns the rendering style option that is on the shading sub-builder Return type: NXOpen.Preferences.ShadingRenderingStyleOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenderingStyle
Parameters: renderingStyleOption ( NXOpen.Preferences.ShadingRenderingStyleOption
) – Sets a new rendering style option on the shading sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ShadeTolerance¶
-
ViewStyleShadingBuilder.
ShadeTolerance
¶ Returns or sets the shade tolerance option on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ShadeTolerance
Returns: Returns the shade tolerance option that is on the shading sub-builder Return type: NXOpen.Preferences.ShadingToleranceOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadeTolerance
Parameters: shadeToleranceOption ( NXOpen.Preferences.ShadingToleranceOption
) – Sets a new shade tolerance option on the shading sub-builderNew in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
ShininessScale¶
-
ViewStyleShadingBuilder.
ShininessScale
¶ Returns or sets the shininess scale data on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
ShininessScale
Returns: Returns the shininess scale that is on the shading sub-builder Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShininessScale
Parameters: shininessScaleData (float) – Sets a new shininess scale on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
TwoSidedLight¶
-
ViewStyleShadingBuilder.
TwoSidedLight
¶ Returns or sets the two sided light toggle on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
TwoSidedLight
Returns: Returns the two sided light toggle value that is on the shading sub-builder Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TwoSidedLight
Parameters: twoSidedLightToggle (bool) – Sets a new two sided light toggle value on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
VisibleWireframeColor¶
-
ViewStyleShadingBuilder.
VisibleWireframeColor
¶ Returns or sets the visible wireframe color on the SHADING tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
VisibleWireframeColor
Returns: Returns the visible wireframe color that is on the shading sub-builder Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleWireframeColor
Parameters: visibleWireframeColor (Id) – Sets a new visible wireframe color on the shading sub-builder New in version NX6.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ViewStyleShadingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.