ViewStyleOrientationBuilder Class¶
-
class
NXOpen.Drawings.
ViewStyleOrientationBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the ORIENTATION tab on the View Style Dialog (Drawings.
ViewStyleOrientationBuilder)
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
HingeLine | Returns the view hinge line definition on the ORIENTATION tab of the View Style Dialog |
Ovt | Returns the view orientation definition on the ORIENTATION tab of the View Style Dialog |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
HingeLine¶
-
ViewStyleOrientationBuilder.
HingeLine
¶ Returns the view hinge line definition on the ORIENTATION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
HingeLine
Returns: Returns the view hinge line definition that is on the style orientation sub-builder Return type: NXOpen.Drawings.HingeLineBuilder
New in version NX6.0.0.
License requirements: None.
Ovt¶
-
ViewStyleOrientationBuilder.
Ovt
¶ Returns the view orientation definition on the ORIENTATION tab of the View Style Dialog
-------------------------------------
Getter Method
Signature
Ovt
Returns: Returns the view orientation definition that is on the style orientation sub-builder Return type: NXOpen.Drawings.OvtBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ViewStyleOrientationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.