MirrorCertificationBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
A
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder
used to create or edit a vehicle designNXOpen.Features.VehicleDesign.MirrorCertification
feature.To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateMirrorCertificationBuilder()
Default values.
Property Value AllowHeadAndEyeRotation 1 ConvexRadius.Value 0 (millimeters part), 0 (inches part) DeviateFromStandard 0 DriverSideStandard UsaCanadaFmvss111Cmvsss111 EyeMethod MaximumDistance EyePointMethod ByHipPoint EyellipsePercentile Percentile95 GenerateValidationLogFile 0 InfiniteDistance.Value 0 (millimeters part), 0 (inches part) InsideStandard UsaCanadaFmvss111Cmvsss111 InstructionFieldPosition OnTargetWall InstructionFieldType Triangle Location Inside MirrorOrientation AutoRotation MirrorType Planar PassengerSideStandard UsaCanadaFmvss111Cmvsss111 RotatedAngleY.Value 0 RotatedAngleZ.Value 0 ShowRays 1 ShowVisionCone None TargetDistance.Value 0 (millimeters part), 0 (inches part) TargetDistanceFar.Value 0 (millimeters part), 0 (inches part) TargetWidthAngular.Value 0 TargetWidthLength.Value 0 (millimeters part), 0 (inches part) TargetWidthLengthFar.Value 0 (millimeters part), 0 (inches part) UseEyeFrom WorkPart UseLoadingSpecifiedByStandard 1 ViewValidationResults 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AllowHeadAndEyeRotation | Returns or sets the indication if the head and eye rotation is allowed. |
BackliteWindshieldFace | Returns the backlite windshield face representing the rear window (backlite) day light opening (DLO). |
BackliteWindshieldFacetBodies | Returns the backlite windshield facet body representing the rear window (backlite) day light opening (DLO). |
BezelCurve | Returns the bezel curve representing the inside perimeter of the closed protective cover (or shell) around a mirror and must be a closed loop of curves. |
ConvexRadius | Returns the convex radius of the spherial mirror. |
DeviateFromStandard | Returns or sets the indication if the target values are deviated from standard. |
DriverSideFacetBodies | Returns the facet body that represents the mirror surface at driver side. |
DriverSideMirrorFace | Returns the face that represents the mirror surface at driver side. |
DriverSideStandard | Returns or sets the standard for the driver side mirror. |
EyeComponent | Returns the component part that contains the eye. |
EyeMethod | Returns or sets the method to calculate the eye location based on the distance from the eyellipse to the mirror pivot. |
EyeMirrorRestrictions | Returns the faces representing the restrictions between the eye and the mirror. |
EyeMirrorRestrictionsFacetBodies | Returns the facet bodies representing the restrictions between the eye and the mirror. |
EyePointMethod | Returns or sets the method to define the eye point. |
Eyellipse | Returns or sets the eyellipse feature name used for mirror certification. |
EyellipsePercentile | Returns or sets the eyellipse percentile that will be used for mirror certification. |
GeneralColor | Returns or sets the color applied to the general output geometries. |
GenerateValidationLogFile | Returns or sets the indication if the validation log file is generated. |
GroundWidePoint | Returns or sets the ground wide point representing the widest position of the vehicle body at the ground level. |
HipPoint | Returns or sets the hip point of the driver. |
InfiniteDistance | Returns the infinite distance to the eye behind the vehicle. |
InsideStandard | Returns or sets the standard for the inside mirror. |
InstructionFieldPosition | Returns or sets the instruction field position, on wall or road. |
InstructionFieldType | Returns or sets the instruction field type, triangle or rectangle. |
LeftEyeColor | Returns or sets the color applied to the left eye vision geometries for the driver or passenger side mirror. |
LeftEyeDownColor | Returns or sets the color applied to the left eye down-vision geometries for the inside mirror. |
LeftEyeUpColor | Returns or sets the color applied to the left eye up-vision geometries for the inside mirror. |
Loading | Returns or sets the loading applied to the vehicle for mirror certification. |
Location | Returns or sets the mirror location. |
MirrorFacetBodies | Returns the facet body that represents the closed mirror profile. |
MirrorOrientation | Returns or sets the mirror orientation method. |
MirrorSurface | Returns the face that represents the closed mirror profile. |
MirrorTargetRestrictions | Returns the faces representing the restrictions between the mirror and the target plane. |
MirrorTargetRestrictionsFacetBodies | Returns the facet body representing the restrictions between the mirror and the target plane. |
MirrorType | Returns or sets the mirror surface type, planar or spherical. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PassengerSideStandard | Returns or sets the standard for passenger side mirror. |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PivotPoint | Returns or sets the pivot point about which the mirror rotates. |
PrimePoint | Returns or sets the prime point representing the highest inboard point on the mirror, which defines the horizontal ray (in side view) parallel to vehicle centerline (in top view). |
RightEyeColor | Returns or sets the color applied to the right eye vision geometries for the driver or passenger side mirror. |
RightEyeDownColor | Returns or sets the color applied to the right eye down-vision geometries for the inside mirror. |
RightEyeUpColor | Returns or sets the color applied to the right eye up-vision geometries for the inside mirror. |
RotatedAngleY | Returns the rotated angle about Y axis. |
RotatedAngleZ | Returns the rotated angle about Z axis. |
ShowRays | Returns or sets the indication if the vision rays are created. |
ShowVisionCone | Returns or sets the indication if the vision cone is shown. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetDistance | Returns the target distance to the eye behind the vehicle, which is defined in the standard. |
TargetDistanceFar | Returns the far target distance to the eye behind the vehicle, which is defined in the standard. |
TargetWidthAngular | Returns the target vision angle, which is defined in the standard. |
TargetWidthLength | Returns the target width at the target distance position, which is defined in the standard. |
TargetWidthLengthFar | Returns the target width at the far target distance position, which is defined in the standard. |
UseEyeFrom | Returns or sets the part that the eye is from. |
UseLoadingSpecifiedByStandard | Returns or sets the flag to indicate if the loading specified by the standard will be used. |
ViewValidationResults | Returns or sets the indication if the packaging validation gadget is invoked to view the results. |
WheelProtrusionPoint | Returns or sets the wheel protrusion point used to calculate close targets near the rear axle centerline. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreatePointWithBaseDataSGRPExpression | Create a point according to Base Data SGRP expressions |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetUserRemarks | Gets the user remarks with the feature. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetUserRemarks | Sets the user remarks with the feature. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MirrorCertificationBuilderDriverSideStandardsType Enumeration | Used to indicate the standard for the driver mirror. |
MirrorCertificationBuilderEyeFromOptionType Enumeration | Used to indicate what part the eye is from. |
MirrorCertificationBuilderEyeMethodType Enumeration | Used to indicate the method to calculate the eye location based on the distance from the eyellipse to the mirror pivot. |
MirrorCertificationBuilderEyePointMethodType Enumeration | Used to indicate the method to define the eye point. |
MirrorCertificationBuilderEyellipsePercentileType Enumeration | Used to indicate the eyellipse percentile that is used in mirror certification. |
MirrorCertificationBuilderInsideStandardsType Enumeration | Used to indicate the standard for the inside mirror. |
MirrorCertificationBuilderInstructionFieldPositionType Enumeration | Used to indicate the postion where the instruction field will be. |
MirrorCertificationBuilderInstructionFieldsType Enumeration | Used to indicate the shape type of the instruction field. |
MirrorCertificationBuilderLocationType Enumeration | Used to indicate the mirror location. |
MirrorCertificationBuilderMirrorOrientationType Enumeration | Used to indicate the method to rotate mirror. |
MirrorCertificationBuilderMirrorSurfaceType Enumeration | Used to indicate the mirror surface type. |
MirrorCertificationBuilderPassengerSideStandardsType Enumeration | Used to indicate the standard for the passenger mirror. |
MirrorCertificationBuilderShowVisionConeType Enumeration | Used to indicate what vision cone will be shown. |
Property Detail¶
AllowHeadAndEyeRotation¶
-
MirrorCertificationBuilder.
AllowHeadAndEyeRotation
¶ Returns or sets the indication if the head and eye rotation is allowed.
-------------------------------------
Getter Method
Signature
AllowHeadAndEyeRotation
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllowHeadAndEyeRotation
Parameters: allowHeadAndEyeRotation (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
BackliteWindshieldFace¶
-
MirrorCertificationBuilder.
BackliteWindshieldFace
¶ Returns the backlite windshield face representing the rear window (backlite) day light opening (DLO).
-------------------------------------
Getter Method
Signature
BackliteWindshieldFace
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
BackliteWindshieldFacetBodies¶
-
MirrorCertificationBuilder.
BackliteWindshieldFacetBodies
¶ Returns the backlite windshield facet body representing the rear window (backlite) day light opening (DLO).
-------------------------------------
Getter Method
Signature
BackliteWindshieldFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
BezelCurve¶
-
MirrorCertificationBuilder.
BezelCurve
¶ Returns the bezel curve representing the inside perimeter of the closed protective cover (or shell) around a mirror and must be a closed loop of curves.
-------------------------------------
Getter Method
Signature
BezelCurve
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
ConvexRadius¶
-
MirrorCertificationBuilder.
ConvexRadius
¶ Returns the convex radius of the spherial mirror.
-------------------------------------
Getter Method
Signature
ConvexRadius
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
DeviateFromStandard¶
-
MirrorCertificationBuilder.
DeviateFromStandard
¶ Returns or sets the indication if the target values are deviated from standard.
-------------------------------------
Getter Method
Signature
DeviateFromStandard
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeviateFromStandard
Parameters: deviateFromStandard (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
DriverSideFacetBodies¶
-
MirrorCertificationBuilder.
DriverSideFacetBodies
¶ Returns the facet body that represents the mirror surface at driver side.
-------------------------------------
Getter Method
Signature
DriverSideFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
DriverSideMirrorFace¶
-
MirrorCertificationBuilder.
DriverSideMirrorFace
¶ Returns the face that represents the mirror surface at driver side.
-------------------------------------
Getter Method
Signature
DriverSideMirrorFace
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
DriverSideStandard¶
-
MirrorCertificationBuilder.
DriverSideStandard
¶ Returns or sets the standard for the driver side mirror.
-------------------------------------
Getter Method
Signature
DriverSideStandard
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderDriverSideStandardsType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DriverSideStandard
Parameters: driverSideStandard ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderDriverSideStandardsType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
EyeComponent¶
-
MirrorCertificationBuilder.
EyeComponent
¶ Returns the component part that contains the eye.
-------------------------------------
Getter Method
Signature
EyeComponent
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX9.0.0.
License requirements: None.
EyeMethod¶
-
MirrorCertificationBuilder.
EyeMethod
¶ Returns or sets the method to calculate the eye location based on the distance from the eyellipse to the mirror pivot.
-------------------------------------
Getter Method
Signature
EyeMethod
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyeMethodType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyeMethod
Parameters: eyeMethod ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyeMethodType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
EyeMirrorRestrictions¶
-
MirrorCertificationBuilder.
EyeMirrorRestrictions
¶ Returns the faces representing the restrictions between the eye and the mirror.
-------------------------------------
Getter Method
Signature
EyeMirrorRestrictions
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
EyeMirrorRestrictionsFacetBodies¶
-
MirrorCertificationBuilder.
EyeMirrorRestrictionsFacetBodies
¶ Returns the facet bodies representing the restrictions between the eye and the mirror.
-------------------------------------
Getter Method
Signature
EyeMirrorRestrictionsFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
EyePointMethod¶
-
MirrorCertificationBuilder.
EyePointMethod
¶ Returns or sets the method to define the eye point.
-------------------------------------
Getter Method
Signature
EyePointMethod
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyePointMethodType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyePointMethod
Parameters: eyePointMethod ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyePointMethodType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Eyellipse¶
-
MirrorCertificationBuilder.
Eyellipse
¶ Returns or sets the eyellipse feature name used for mirror certification.
-------------------------------------
Getter Method
Signature
Eyellipse
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Eyellipse
Parameters: eyellipse (str) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
EyellipsePercentile¶
-
MirrorCertificationBuilder.
EyellipsePercentile
¶ Returns or sets the eyellipse percentile that will be used for mirror certification.
-------------------------------------
Getter Method
Signature
EyellipsePercentile
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyellipsePercentileType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyellipsePercentile
Parameters: eyellipsePercentile ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyellipsePercentileType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
GeneralColor¶
-
MirrorCertificationBuilder.
GeneralColor
¶ Returns or sets the color applied to the general output geometries.
-------------------------------------
Getter Method
Signature
GeneralColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeneralColor
Parameters: generalColor (Id) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
GenerateValidationLogFile¶
-
MirrorCertificationBuilder.
GenerateValidationLogFile
¶ Returns or sets the indication if the validation log file is generated.
-------------------------------------
Getter Method
Signature
GenerateValidationLogFile
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerateValidationLogFile
Parameters: generateValidationLogFile (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
GroundWidePoint¶
-
MirrorCertificationBuilder.
GroundWidePoint
¶ Returns or sets the ground wide point representing the widest position of the vehicle body at the ground level.
-------------------------------------
Getter Method
Signature
GroundWidePoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GroundWidePoint
Parameters: groundWidePoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
HipPoint¶
-
MirrorCertificationBuilder.
HipPoint
¶ Returns or sets the hip point of the driver.
-------------------------------------
Getter Method
Signature
HipPoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HipPoint
Parameters: hipPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
InfiniteDistance¶
-
MirrorCertificationBuilder.
InfiniteDistance
¶ Returns the infinite distance to the eye behind the vehicle.
-------------------------------------
Getter Method
Signature
InfiniteDistance
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
InsideStandard¶
-
MirrorCertificationBuilder.
InsideStandard
¶ Returns or sets the standard for the inside mirror.
-------------------------------------
Getter Method
Signature
InsideStandard
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInsideStandardsType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsideStandard
Parameters: insideStandard ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInsideStandardsType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
InstructionFieldPosition¶
-
MirrorCertificationBuilder.
InstructionFieldPosition
¶ Returns or sets the instruction field position, on wall or road.
-------------------------------------
Getter Method
Signature
InstructionFieldPosition
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldPositionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InstructionFieldPosition
Parameters: instructionFieldPosition ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldPositionType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
InstructionFieldType¶
-
MirrorCertificationBuilder.
InstructionFieldType
¶ Returns or sets the instruction field type, triangle or rectangle.
-------------------------------------
Getter Method
Signature
InstructionFieldType
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldsType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InstructionFieldType
Parameters: instructionFieldType ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldsType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
LeftEyeColor¶
-
MirrorCertificationBuilder.
LeftEyeColor
¶ Returns or sets the color applied to the left eye vision geometries for the driver or passenger side mirror.
-------------------------------------
Getter Method
Signature
LeftEyeColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LeftEyeColor
Parameters: leftEyeColor (Id) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
LeftEyeDownColor¶
-
MirrorCertificationBuilder.
LeftEyeDownColor
¶ Returns or sets the color applied to the left eye down-vision geometries for the inside mirror.
-------------------------------------
Getter Method
Signature
LeftEyeDownColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LeftEyeDownColor
Parameters: leftEyeDownColor (Id) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
LeftEyeUpColor¶
-
MirrorCertificationBuilder.
LeftEyeUpColor
¶ Returns or sets the color applied to the left eye up-vision geometries for the inside mirror.
-------------------------------------
Getter Method
Signature
LeftEyeUpColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LeftEyeUpColor
Parameters: leftEyeUpColor (Id) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Loading¶
-
MirrorCertificationBuilder.
Loading
¶ Returns or sets the loading applied to the vehicle for mirror certification.
-------------------------------------
Getter Method
Signature
Loading
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading
Parameters: loading (str) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Location¶
-
MirrorCertificationBuilder.
Location
¶ Returns or sets the mirror location.
-------------------------------------
Getter Method
Signature
Location
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderLocationType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Location
Parameters: location ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderLocationType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
MirrorFacetBodies¶
-
MirrorCertificationBuilder.
MirrorFacetBodies
¶ Returns the facet body that represents the closed mirror profile.
-------------------------------------
Getter Method
Signature
MirrorFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
MirrorOrientation¶
-
MirrorCertificationBuilder.
MirrorOrientation
¶ Returns or sets the mirror orientation method.
-------------------------------------
Getter Method
Signature
MirrorOrientation
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorOrientationType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MirrorOrientation
Parameters: mirrorOrientation ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorOrientationType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
MirrorSurface¶
-
MirrorCertificationBuilder.
MirrorSurface
¶ Returns the face that represents the closed mirror profile.
-------------------------------------
Getter Method
Signature
MirrorSurface
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
MirrorTargetRestrictions¶
-
MirrorCertificationBuilder.
MirrorTargetRestrictions
¶ Returns the faces representing the restrictions between the mirror and the target plane.
-------------------------------------
Getter Method
Signature
MirrorTargetRestrictions
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
MirrorTargetRestrictionsFacetBodies¶
-
MirrorCertificationBuilder.
MirrorTargetRestrictionsFacetBodies
¶ Returns the facet body representing the restrictions between the mirror and the target plane.
-------------------------------------
Getter Method
Signature
MirrorTargetRestrictionsFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
MirrorType¶
-
MirrorCertificationBuilder.
MirrorType
¶ Returns or sets the mirror surface type, planar or spherical.
-------------------------------------
Getter Method
Signature
MirrorType
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorSurfaceType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MirrorType
Parameters: mirrorType ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorSurfaceType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PassengerSideStandard¶
-
MirrorCertificationBuilder.
PassengerSideStandard
¶ Returns or sets the standard for passenger side mirror.
-------------------------------------
Getter Method
Signature
PassengerSideStandard
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderPassengerSideStandardsType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PassengerSideStandard
Parameters: passengerSideStandard ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderPassengerSideStandardsType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PivotPoint¶
-
MirrorCertificationBuilder.
PivotPoint
¶ Returns or sets the pivot point about which the mirror rotates.
-------------------------------------
Getter Method
Signature
PivotPoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PivotPoint
Parameters: pivotPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PrimePoint¶
-
MirrorCertificationBuilder.
PrimePoint
¶ Returns or sets the prime point representing the highest inboard point on the mirror, which defines the horizontal ray (in side view) parallel to vehicle centerline (in top view).
-------------------------------------
Getter Method
Signature
PrimePoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrimePoint
Parameters: primePoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RightEyeColor¶
-
MirrorCertificationBuilder.
RightEyeColor
¶ Returns or sets the color applied to the right eye vision geometries for the driver or passenger side mirror.
-------------------------------------
Getter Method
Signature
RightEyeColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RightEyeColor
Parameters: rightEyeColor (Id) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RightEyeDownColor¶
-
MirrorCertificationBuilder.
RightEyeDownColor
¶ Returns or sets the color applied to the right eye down-vision geometries for the inside mirror.
-------------------------------------
Getter Method
Signature
RightEyeDownColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RightEyeDownColor
Parameters: rightEyeDownColor (Id) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RightEyeUpColor¶
-
MirrorCertificationBuilder.
RightEyeUpColor
¶ Returns or sets the color applied to the right eye up-vision geometries for the inside mirror.
-------------------------------------
Getter Method
Signature
RightEyeUpColor
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RightEyeUpColor
Parameters: rightEyeUpColor (Id) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RotatedAngleY¶
-
MirrorCertificationBuilder.
RotatedAngleY
¶ Returns the rotated angle about Y axis.
-------------------------------------
Getter Method
Signature
RotatedAngleY
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
RotatedAngleZ¶
-
MirrorCertificationBuilder.
RotatedAngleZ
¶ Returns the rotated angle about Z axis.
-------------------------------------
Getter Method
Signature
RotatedAngleZ
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
ShowRays¶
-
MirrorCertificationBuilder.
ShowRays
¶ Returns or sets the indication if the vision rays are created.
-------------------------------------
Getter Method
Signature
ShowRays
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowRays
Parameters: showRays (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowVisionCone¶
-
MirrorCertificationBuilder.
ShowVisionCone
¶ Returns or sets the indication if the vision cone is shown.
-------------------------------------
Getter Method
Signature
ShowVisionCone
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderShowVisionConeType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowVisionCone
Parameters: showVisionCone ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderShowVisionConeType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
TargetDistance¶
-
MirrorCertificationBuilder.
TargetDistance
¶ Returns the target distance to the eye behind the vehicle, which is defined in the standard.
-------------------------------------
Getter Method
Signature
TargetDistance
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
TargetDistanceFar¶
-
MirrorCertificationBuilder.
TargetDistanceFar
¶ Returns the far target distance to the eye behind the vehicle, which is defined in the standard.
-------------------------------------
Getter Method
Signature
TargetDistanceFar
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
TargetWidthAngular¶
-
MirrorCertificationBuilder.
TargetWidthAngular
¶ Returns the target vision angle, which is defined in the standard.
-------------------------------------
Getter Method
Signature
TargetWidthAngular
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
TargetWidthLength¶
-
MirrorCertificationBuilder.
TargetWidthLength
¶ Returns the target width at the target distance position, which is defined in the standard.
-------------------------------------
Getter Method
Signature
TargetWidthLength
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
TargetWidthLengthFar¶
-
MirrorCertificationBuilder.
TargetWidthLengthFar
¶ Returns the target width at the far target distance position, which is defined in the standard.
-------------------------------------
Getter Method
Signature
TargetWidthLengthFar
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
UseEyeFrom¶
-
MirrorCertificationBuilder.
UseEyeFrom
¶ Returns or sets the part that the eye is from.
-------------------------------------
Getter Method
Signature
UseEyeFrom
Returns: Return type: NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyeFromOptionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseEyeFrom
Parameters: useEyeFrom ( NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyeFromOptionType
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UseLoadingSpecifiedByStandard¶
-
MirrorCertificationBuilder.
UseLoadingSpecifiedByStandard
¶ Returns or sets the flag to indicate if the loading specified by the standard will be used.
-------------------------------------
Getter Method
Signature
UseLoadingSpecifiedByStandard
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseLoadingSpecifiedByStandard
Parameters: useLoadingSpecifiedByStandard (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ViewValidationResults¶
-
MirrorCertificationBuilder.
ViewValidationResults
¶ Returns or sets the indication if the packaging validation gadget is invoked to view the results.
-------------------------------------
Getter Method
Signature
ViewValidationResults
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ViewValidationResults
Parameters: viewValidationResults (bool) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
WheelProtrusionPoint¶
-
MirrorCertificationBuilder.
WheelProtrusionPoint
¶ Returns or sets the wheel protrusion point used to calculate close targets near the rear axle centerline.
-------------------------------------
Getter Method
Signature
WheelProtrusionPoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WheelProtrusionPoint
Parameters: wheelProtrusionPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Method Detail¶
CreatePointWithBaseDataSGRPExpression¶
-
MirrorCertificationBuilder.
CreatePointWithBaseDataSGRPExpression
¶ Create a point according to Base Data SGRP expressions
Signature
CreatePointWithBaseDataSGRPExpression()
Returns: Return type: NXOpen.Point
New in version NX11.0.1.
License requirements: None.
GetUserRemarks¶
-
MirrorCertificationBuilder.
GetUserRemarks
¶ Gets the user remarks with the feature.
Signature
GetUserRemarks()
Returns: Return type: list of str New in version NX9.0.0.
License requirements: None.
SetUserRemarks¶
-
MirrorCertificationBuilder.
SetUserRemarks
¶ Sets the user remarks with the feature.
Signature
SetUserRemarks(userRemarks)
Parameters: userRemarks (list of str) – New in version NX9.0.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Validate¶
-
MirrorCertificationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.