MirrorCertificationBuilderEyeFromOptionType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.EyeFromOptionType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyeFromOptionType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderEyeFromOptionType
¶ Bases:
object
Used to indicate what part the eye is from.
Enum Members
Enum Member Enum Member Description WorkPart Represents eyellipse feature is from work part RootPart Represents eyellipse feature is from root part OtherComponent Represents eyellipse feature is from the other component Part -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-