MirrorCertificationBuilderInstructionFieldsType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.InstructionFieldsType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderInstructionFieldsType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderInstructionFieldsType
¶ Bases:
object
Used to indicate the shape type of the instruction field.
Enum Members
Enum Member Enum Member Description Triangle Represents that the triangle Instruction field will be created Rectangle Represents that the rectangle Instruction field will be created -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-