MirrorCertificationBuilderShowVisionConeType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.ShowVisionConeType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderShowVisionConeType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderShowVisionConeType
¶ Bases:
object
Used to indicate what vision cone will be shown.
Enum Members
Enum Member Enum Member Description NotSet Represents the vision cones aren’t shown All Represents both of Eye-Mirror and Mirror Target vision cones are shown EyeToMirror Represents only Eye-Mirror vision cone is shown MirrorToTarget Represents only Mirror-Target vision cone is shown -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-