MirrorCertificationBuilderPassengerSideStandardsType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.PassengerSideStandardsType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderPassengerSideStandardsType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderPassengerSideStandardsType
¶ Bases:
object
Used to indicate the standard for the passenger mirror.
Enum Members
Enum Member Enum Member Description UsaCanadaFmvss111Cmvsss111 Represents USA - Canada : FMVSS111 - CMVSSS111 standard EuropeM1n1ClassiiiMirror200397EcEcer4602 Represents Europe (M1/N1_Class III Mirror) : 2003/97/EC - ECE R46.02 standard EuropeM1n1Only71127EuEcer4601Superceded Represents Europe (M1/N1 only) : 71/127/EU - ECE R46.01 (Superceded ) standard EuropeNotM1n171127EuEcer4601Superceded Represents Europe (Not M1/N1) : 71/127/EU - ECE R46.01 : (Superceded ) standard JapanArticle44Trias29Trias39 Represents Japan : Article 44/TRIAS 29/TRIAS 39 standard AustraliaAdr1402 Represents Australia : ADR 14/02 standard SaudiArabiaGulfStatesSsa770771Gs421442 Represents Saudi Arabia - Gulf States : SSA 770/771 GS 421/442 standard ChinaM1n1OnlyGb150842006 Represents China (M1/N1 only) : GB 15084 - 2006 standard ChinaNotM1n1Gb150842006 Represents China (Not M1/N1) : GB 15084 - 2006 standard -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-