MirrorCertificationBuilderEyePointMethodType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.EyePointMethodType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderEyePointMethodType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderEyePointMethodType
¶ Bases:
object
Used to indicate the method to define the eye point.
Enum Members
Enum Member Enum Member Description ByEceVisionPointsFeature Represents using ECE Vision Point feature to get eye point ByHipPoint Represents using Hip Point to calculate the eye point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-