MirrorCertificationBuilderMirrorOrientationType Enumeration¶
NXOpen.Features.VehicleDesign.MirrorCertificationBuilder.MirrorOrientationType is an alias for NXOpen.Features.VehicleDesign.MirrorCertificationBuilderMirrorOrientationType
-
class
NXOpen.Features.VehicleDesign.
MirrorCertificationBuilderMirrorOrientationType
¶ Bases:
object
Used to indicate the method to rotate mirror.
Enum Members
Enum Member Enum Member Description AutoRotation Represents that the mirror will be rotated automatically InteractiveAdjustment Represents that the mirror will be rotated interactively -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-