ExtractFaceBuilder Class¶
-
class
NXOpen.Features.
ExtractFaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ExtractFace
builder.Inputs to this class can be convergent objects.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateExtractFaceBuilder()
Default values.
Property Value AngleTolerance 45.0 Associative True CopyThreads True DeleteHoles False FixAtCurrentTimestamp False InheritDisplayProperties False IsPsmOutputBody false MakePositionIndependent False ReplacementAssistant.OneToOne True New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle Tolerance |
Associative | Returns or sets the option that specifies whether the extract face operation is associative |
BodyReverseDirection | Returns or sets the option to specify if the extracted faces should have the face normals reversed from the selected input bodies. |
BodyToExtract | Returns the bodies |
BoundaryFaces | Returns the boundary faces |
CopyThreads | Returns or sets the copy threads option |
DeleteHoles | Returns or sets the option to specify if holes should be deleted from the extracted faces |
ExtractBodyCollector | Returns a collection of bodies to extract |
FaceChain | Returns the face chain containing the faces to extract |
FaceOption | Returns or sets the face option type |
FaceReverseDirection | Returns or sets the option specifying whether to reverse the face normals for the extracted faces. |
FacesToExtract | Returns the faces |
FeatureOption | Returns or sets the feature option type |
FixAtCurrentTimestamp | Returns or sets the option specifying whether to fix the extract face operation at the current timestamp |
FrecAtTimeStamp | Returns or sets the option specifying if the results from this builder should be associated |
HideOriginal | Returns or sets the option to specify if the original faces should be hidden |
InheritDisplayProperties | Returns or sets the inherit display properties from source option |
IsPsmOutputBody | Returns or sets the PSM Body Output option |
MakePositionIndependent | Returns or sets the option to specify that the extracted faces should be position independent |
ObjectToExtract | Returns a list of the extracted objects. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
ParentPart | Returns or sets the source part type |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReplacementAssistant | Returns the Replacement Assistant builder. |
SeedFace | Returns the seed face for the face chain |
SeedReverseDirection | Returns or sets the option that specifies whether to reverse the face normals of the extracted faces relative to the seed face chain |
SourcePartOccurrence | Returns or sets the source part occurrence |
SurfaceType | Returns or sets the surface type |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TraverseInteriorEdges | Returns or sets the traverse interior edges |
Type | Returns or sets the type |
UseTangentEdgeAngles | Returns or sets the use tangent angles |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitCreateOnTheFly | Commits the feature and set create on the fly flag |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipFaceChainDirectionSense | Flip the face chain direction sense |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFaceChainDirectionSense | Returns the face chain direction sense for a given face in the face chain |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetProductInterfaceObjects | Gets selected product interface objects |
GetSourcePartOccurrences | Gets source part occurrences |
GetWaveLinkInformation | Prints wave browser type information about link |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RecreateVectorOfHelpDirVector | Causes the recreation of vector for help dir |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetProductInterfaceObjects | Sets selected product interface objects |
SetSourcePartOccurrences | Sets source part occurrences |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ExtractFaceBuilderExtractType Enumeration | enum for feature type being extracted |
ExtractFaceBuilderFaceOptionType Enumeration | enum for face option type |
ExtractFaceBuilderFaceSurfaceType Enumeration | type of resulting surface |
ExtractFaceBuilderFeatureOptionType Enumeration | enum for feature option type |
ExtractFaceBuilderParentPartType Enumeration | enum for scope of part |
Property Detail¶
AngleTolerance¶
-
ExtractFaceBuilder.
AngleTolerance
¶ Returns or sets the angle Tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
Associative¶
-
ExtractFaceBuilder.
Associative
¶ Returns or sets the option that specifies whether the extract face operation is associative
-------------------------------------
Getter Method
Signature
Associative
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Associative
Parameters: associative (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
BodyReverseDirection¶
-
ExtractFaceBuilder.
BodyReverseDirection
¶ Returns or sets the option to specify if the extracted faces should have the face normals reversed from the selected input bodies.
-------------------------------------
Getter Method
Signature
BodyReverseDirection
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BodyReverseDirection
Parameters: bodyNormal (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
BodyToExtract¶
-
ExtractFaceBuilder.
BodyToExtract
¶ Returns the bodies
-------------------------------------
Getter Method
Signature
BodyToExtract
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.ExtractFaceBuilder.ExtractBodyCollector()
instead.License requirements: None.
BoundaryFaces¶
-
ExtractFaceBuilder.
BoundaryFaces
¶ Returns the boundary faces
-------------------------------------
Getter Method
Signature
BoundaryFaces
Returns: Return type: NXOpen.SelectFaceList
New in version NX5.0.0.
License requirements: None.
CopyThreads¶
-
ExtractFaceBuilder.
CopyThreads
¶ Returns or sets the copy threads option
-------------------------------------
Getter Method
Signature
CopyThreads
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyThreads
Parameters: copyThreads (bool) – New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
DeleteHoles¶
-
ExtractFaceBuilder.
DeleteHoles
¶ Returns or sets the option to specify if holes should be deleted from the extracted faces
-------------------------------------
Getter Method
Signature
DeleteHoles
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeleteHoles
Parameters: deleteHoles (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
ExtractBodyCollector¶
-
ExtractFaceBuilder.
ExtractBodyCollector
¶ Returns a collection of bodies to extract
-------------------------------------
Getter Method
Signature
ExtractBodyCollector
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
FaceChain¶
-
ExtractFaceBuilder.
FaceChain
¶ Returns the face chain containing the faces to extract
-------------------------------------
Getter Method
Signature
FaceChain
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
FaceOption¶
-
ExtractFaceBuilder.
FaceOption
¶ Returns or sets the face option type
-------------------------------------
Getter Method
Signature
FaceOption
Returns: Return type: NXOpen.Features.ExtractFaceBuilderFaceOptionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceOption
Parameters: faceOptionType ( NXOpen.Features.ExtractFaceBuilderFaceOptionType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
FaceReverseDirection¶
-
ExtractFaceBuilder.
FaceReverseDirection
¶ Returns or sets the option specifying whether to reverse the face normals for the extracted faces.
-------------------------------------
Getter Method
Signature
FaceReverseDirection
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceReverseDirection
Parameters: faceNormal (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
FacesToExtract¶
-
ExtractFaceBuilder.
FacesToExtract
¶ Returns the faces
-------------------------------------
Getter Method
Signature
FacesToExtract
Returns: Return type: NXOpen.SelectFaceList
New in version NX5.0.0.
Deprecated since version NX7.5.0: Use
NXOpen.Features.ExtractFaceBuilder.ObjectToExtract()
instead.License requirements: None.
FeatureOption¶
-
ExtractFaceBuilder.
FeatureOption
¶ Returns or sets the feature option type
-------------------------------------
Getter Method
Signature
FeatureOption
Returns: Return type: NXOpen.Features.ExtractFaceBuilderFeatureOptionType
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureOption
Parameters: featureOptionType ( NXOpen.Features.ExtractFaceBuilderFeatureOptionType
) –New in version NX9.0.3.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
FixAtCurrentTimestamp¶
-
ExtractFaceBuilder.
FixAtCurrentTimestamp
¶ Returns or sets the option specifying whether to fix the extract face operation at the current timestamp
-------------------------------------
Getter Method
Signature
FixAtCurrentTimestamp
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FixAtCurrentTimestamp
Parameters: fixAtTimestamp (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
FrecAtTimeStamp¶
-
ExtractFaceBuilder.
FrecAtTimeStamp
¶ Returns or sets the option specifying if the results from this builder should be associated
-------------------------------------
Getter Method
Signature
FrecAtTimeStamp
Returns: Return type: NXOpen.Features.Feature
New in version NX6.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FrecAtTimeStamp
Parameters: terminalFrec ( NXOpen.Features.Feature
) –New in version NX6.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
HideOriginal¶
-
ExtractFaceBuilder.
HideOriginal
¶ Returns or sets the option to specify if the original faces should be hidden
-------------------------------------
Getter Method
Signature
HideOriginal
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HideOriginal
Parameters: hideOriginal (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
InheritDisplayProperties¶
-
ExtractFaceBuilder.
InheritDisplayProperties
¶ Returns or sets the inherit display properties from source option
-------------------------------------
Getter Method
Signature
InheritDisplayProperties
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InheritDisplayProperties
Parameters: inheritDisplayProperties (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
IsPsmOutputBody¶
-
ExtractFaceBuilder.
IsPsmOutputBody
¶ Returns or sets the PSM Body Output option
-------------------------------------
Getter Method
Signature
IsPsmOutputBody
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsPsmOutputBody
Parameters: psmBodyOutput (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”)
MakePositionIndependent¶
-
ExtractFaceBuilder.
MakePositionIndependent
¶ Returns or sets the option to specify that the extracted faces should be position independent
-------------------------------------
Getter Method
Signature
MakePositionIndependent
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MakePositionIndependent
Parameters: makePositionIndependent (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
ObjectToExtract¶
-
ExtractFaceBuilder.
ObjectToExtract
¶ Returns a list of the extracted objects.
The objects in the list are
NXOpen.Face
objects.-------------------------------------
Getter Method
Signature
ObjectToExtract
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX7.5.0.
License requirements: None.
ParentPart¶
-
ExtractFaceBuilder.
ParentPart
¶ Returns or sets the source part type
-------------------------------------
Getter Method
Signature
ParentPart
Returns: Return type: NXOpen.Features.ExtractFaceBuilderParentPartType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentPart
Parameters: parentPart ( NXOpen.Features.ExtractFaceBuilderParentPartType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
ReplacementAssistant¶
-
ExtractFaceBuilder.
ReplacementAssistant
¶ Returns the Replacement Assistant builder.
Call Enter() to enter or re-enter into the mapping environment. Enter() needs to be executed before invoking any map creation or automatic mapping APIs. The maps inferred internally (internal identifier reuse, inherited from parent and siblings) will be populated when Enter() is executed for the first time after selecting a replacement entity. Call Exit() to exit the mapping environment.
-------------------------------------
Getter Method
Signature
ReplacementAssistant
Returns: Return type: NXOpen.GeometricUtilities.ReplAsstBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
SeedFace¶
-
ExtractFaceBuilder.
SeedFace
¶ Returns the seed face for the face chain
-------------------------------------
Getter Method
Signature
SeedFace
Returns: Return type: NXOpen.SelectFace
New in version NX5.0.0.
License requirements: None.
SeedReverseDirection¶
-
ExtractFaceBuilder.
SeedReverseDirection
¶ Returns or sets the option that specifies whether to reverse the face normals of the extracted faces relative to the seed face chain
-------------------------------------
Getter Method
Signature
SeedReverseDirection
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedReverseDirection
Parameters: seedNormal (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
SourcePartOccurrence¶
-
ExtractFaceBuilder.
SourcePartOccurrence
¶ Returns or sets the source part occurrence
-------------------------------------
Getter Method
Signature
SourcePartOccurrence
Returns: Return type: NXOpen.TaggedObject
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SourcePartOccurrence
Parameters: sourcePartOcc ( NXOpen.TaggedObject
) –New in version NX9.0.0.
License requirements: None.
SurfaceType¶
-
ExtractFaceBuilder.
SurfaceType
¶ Returns or sets the surface type
-------------------------------------
Getter Method
Signature
SurfaceType
Returns: Return type: NXOpen.Features.ExtractFaceBuilderFaceSurfaceType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceType
Parameters: surfaceType ( NXOpen.Features.ExtractFaceBuilderFaceSurfaceType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
TraverseInteriorEdges¶
-
ExtractFaceBuilder.
TraverseInteriorEdges
¶ Returns or sets the traverse interior edges
-------------------------------------
Getter Method
Signature
TraverseInteriorEdges
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TraverseInteriorEdges
Parameters: traverseInteriorEdges (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
Type¶
-
ExtractFaceBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.ExtractFaceBuilderExtractType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.ExtractFaceBuilderExtractType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
UseTangentEdgeAngles¶
-
ExtractFaceBuilder.
UseTangentEdgeAngles
¶ Returns or sets the use tangent angles
-------------------------------------
Getter Method
Signature
UseTangentEdgeAngles
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseTangentEdgeAngles
Parameters: useTangentAngles (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
CommitCreateOnTheFly¶
-
ExtractFaceBuilder.
CommitCreateOnTheFly
¶ Commits the feature and set create on the fly flag
Signature
CommitCreateOnTheFly()
Returns: Return type: NXOpen.Features.Feature
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
FlipFaceChainDirectionSense¶
-
ExtractFaceBuilder.
FlipFaceChainDirectionSense
¶ Flip the face chain direction sense
Signature
FlipFaceChainDirectionSense(face)
Parameters: face ( NXOpen.Face
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
GetFaceChainDirectionSense¶
-
ExtractFaceBuilder.
GetFaceChainDirectionSense
¶ Returns the face chain direction sense for a given face in the face chain
Signature
GetFaceChainDirectionSense(face)
Parameters: face ( NXOpen.Face
) –Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
GetProductInterfaceObjects¶
-
ExtractFaceBuilder.
GetProductInterfaceObjects
¶ Gets selected product interface objects
Signature
GetProductInterfaceObjects()
Returns: items in list Return type: list of NXOpen.Assemblies.ProductInterface.InterfaceObject
New in version NX9.0.0.
License requirements: None.
GetSourcePartOccurrences¶
-
ExtractFaceBuilder.
GetSourcePartOccurrences
¶ Gets source part occurrences
Signature
GetSourcePartOccurrences()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX10.0.0.
License requirements: None.
GetWaveLinkInformation¶
-
ExtractFaceBuilder.
GetWaveLinkInformation
¶ Prints wave browser type information about link
Signature
GetWaveLinkInformation()
Returns: a tuple Return type: A tuple consisting of (info, xformExists, xformOrigin, xformOrientation, xformScale). info is a str. queried wave information xformExists is a bool. true if there is a transform xformOrigin is a NXOpen.Point3d
. transformation origin xformOrientation is aNXOpen.Matrix3x3
. transformation matrix xformScale is a float. transformation scaleNew in version NX6.0.0.
License requirements: wave (“WAVE FUNCTIONALITY”)
RecreateVectorOfHelpDirVector¶
-
ExtractFaceBuilder.
RecreateVectorOfHelpDirVector
¶ Causes the recreation of vector for help dir
Signature
RecreateVectorOfHelpDirVector()
New in version NX7.5.4.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR geometric_tol (“GDT”) OR insp_programming (“INSPECTION PROGRAMMING”)
SetProductInterfaceObjects¶
-
ExtractFaceBuilder.
SetProductInterfaceObjects
¶ Sets selected product interface objects
Signature
SetProductInterfaceObjects(selectedObjects)
Parameters: selectedObjects (list of NXOpen.Assemblies.ProductInterface.InterfaceObject
) – items in listNew in version NX9.0.0.
License requirements: None.
SetSourcePartOccurrences¶
-
ExtractFaceBuilder.
SetSourcePartOccurrences
¶ Sets source part occurrences
Signature
SetSourcePartOccurrences(sourcePartOccurrences)
Parameters: sourcePartOccurrences (list of NXOpen.TaggedObject
) –New in version NX10.0.0.
License requirements: None.
Validate¶
-
ExtractFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.