InterfaceObject Class¶
-
class
NXOpen.Assemblies.ProductInterface.
InterfaceObject
¶ Bases:
NXOpen.NXObject
Represents a Product Interface Object Builder.
It creates a product interface object To create a new instance of this class, use
NXOpen.Assemblies.ProductInterface.ObjectBuilder.AddProductInterfaceObject()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
BreakPIReferencingLinks | Breaks referencing link of PI when usage type changes. |
CheckProductInterfaceObject | Check the invalid state of product interface object |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FixInvalidProductInterfaceObject | Fix the invalid state of product interface object |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetInterfaceUsageType | Returns the usage type of the product interface object |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetProductInterfaceDefiningEntity | Returns the underlying NX object referenced by the input product interface object |
GetProductInterfaceObjectStatus | Returns the status of the input product interface object |
GetProductInterfaceObjectType | Returns the type of the input product interface object |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetRelatedExpressions | Returns all expressions related to the product interface object |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetUserComments | Returns the user comments on the input product interface object |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
InsertRelatedExpressions | Relate expressions to the product interface |
Prints a representation of this object to the system log file. | |
RemoveAllRelatedExpressions | Removes all related expressions from the product interface object |
RemoveProductInterfaceObject | Removes an object from the product interface set; currently supported types are expressions and geometry |
RemoveRelatedExpression | Removes related expression from the product interface object |
RenameProductInterfaceObject | Renames an object from the product interface set |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetInterfaceUsageType | Sets the usage type on the product interface object |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SetUserComments | Sets the user comments on the input product interface object |
Enumerations¶
InterfaceObjectInterfaceUsageType Enumeration | An enum representing product interface usage types |
InterfaceObjectInvalidState Enumeration | Invalid state of problematic product interface object |
Property Detail¶
IsOccurrence¶
-
InterfaceObject.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
InterfaceObject.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
InterfaceObject.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
InterfaceObject.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
InterfaceObject.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
InterfaceObject.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
BreakPIReferencingLinks¶
-
InterfaceObject.
BreakPIReferencingLinks
¶ Breaks referencing link of PI when usage type changes.
When the product interface type changed to input or key performance interface. Break link feature and inter part expression referring to the product interface.
Signature
BreakPIReferencingLinks(usageType)
Parameters: usageType ( NXOpen.Assemblies.ProductInterface.InterfaceObjectInterfaceUsageType
) – usage type to be set on the product interface objectNew in version NX12.0.0.
License requirements: None.
CheckProductInterfaceObject¶
-
InterfaceObject.
CheckProductInterfaceObject
¶ Check the invalid state of product interface object
Signature
CheckProductInterfaceObject()
Returns: The state of product interface object Return type: NXOpen.Assemblies.ProductInterface.InterfaceObjectInvalidState
New in version NX10.0.1.
License requirements: None.
FindObject¶
-
InterfaceObject.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
FixInvalidProductInterfaceObject¶
-
InterfaceObject.
FixInvalidProductInterfaceObject
¶ Fix the invalid state of product interface object
Signature
FixInvalidProductInterfaceObject()
Returns: if true the product interface has an issue and is fixed Return type: bool New in version NX10.0.1.
License requirements: None.
GetInterfaceUsageType¶
-
InterfaceObject.
GetInterfaceUsageType
¶ Returns the usage type of the product interface object
Signature
GetInterfaceUsageType()
Returns: usage type of the product interface object Return type: NXOpen.Assemblies.ProductInterface.InterfaceObjectInterfaceUsageType
New in version NX12.0.0.
License requirements: None.
GetProductInterfaceDefiningEntity¶
-
InterfaceObject.
GetProductInterfaceDefiningEntity
¶ Returns the underlying NX object referenced by the input product interface object
Signature
GetProductInterfaceDefiningEntity()
Returns: nx item referenced by the product interface Return type: NXOpen.NXObject
New in version NX5.0.1.
License requirements: None.
GetProductInterfaceObjectStatus¶
-
InterfaceObject.
GetProductInterfaceObjectStatus
¶ Returns the status of the input product interface object
Signature
GetProductInterfaceObjectStatus()
Returns: status of the product interface object Return type: str New in version NX5.0.1.
License requirements: None.
GetProductInterfaceObjectType¶
-
InterfaceObject.
GetProductInterfaceObjectType
¶ Returns the type of the input product interface object
Signature
GetProductInterfaceObjectType()
Returns: type of the product interface object Return type: str New in version NX5.0.1.
License requirements: None.
GetUserComments¶
-
InterfaceObject.
GetUserComments
¶ Returns the user comments on the input product interface object
Signature
GetUserComments()
Returns: user comments on the product interface object Return type: str New in version NX5.0.1.
License requirements: None.
Print¶
-
InterfaceObject.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveProductInterfaceObject¶
-
InterfaceObject.
RemoveProductInterfaceObject
¶ Removes an object from the product interface set; currently supported types are expressions and geometry
Signature
RemoveProductInterfaceObject()
New in version NX9.0.0.
License requirements: None.
RenameProductInterfaceObject¶
-
InterfaceObject.
RenameProductInterfaceObject
¶ Renames an object from the product interface set
Signature
RenameProductInterfaceObject(name)
Parameters: name (str) – user defined name to be set on the product interface object, if it is empty reset it to default name New in version NX9.0.0.
License requirements: None.
SetInterfaceUsageType¶
-
InterfaceObject.
SetInterfaceUsageType
¶ Sets the usage type on the product interface object
Signature
SetInterfaceUsageType(usageType)
Parameters: usageType ( NXOpen.Assemblies.ProductInterface.InterfaceObjectInterfaceUsageType
) – usage type to be set on the product interface objectNew in version NX12.0.0.
License requirements: None.
SetName¶
-
InterfaceObject.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.