ObjectBuilder Class¶
-
class
NXOpen.Assemblies.ProductInterface.
ObjectBuilder
¶ Bases:
NXOpen.Builder
Represents a Product Interface Object Builder.
It creates a set of product interface objects To create a new instance of this class, use
NXOpen.Assemblies.ProductInterface.Collection.CreateObjectBuilderWithVersion()
Default values.
Property Value PartGeometryCopy.ObjectType BodyCollector New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
MateSetting | Returns or sets the current rule setting for use during creation of mating conditions |
PartGeometryCopy | Returns the part geometry copy |
Tag | Returns the Tag for this object. |
WaveSetting | Returns or sets the current rule setting for use during creation of WAVE geomtery and interpart expressions |
Methods¶
Method | Description |
---|---|
AddProductInterface | Adds an object to the product interface; currently supported types are expressions and geometry. |
AddProductInterfaceObject | Adds an object to the product interface; currently supported types are expressions and geometry |
AddProductInterfaceObject1 | Adds an object to the product interface; currently supported types are expressions and geometry |
AddProductInterfaceObject2 | Adds an object to the product interface; currently supported types are expressions and geometry. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditProductInterfaceObject | Edits a product interface object |
EditProductInterfaceObject1 | Edits a product interface object with interface object type . |
GetBuilderVersion | Gets the version of this builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
QueryProductInterfaceObjects | Returns a list of product interface objects in the part |
RemoveProductInterfaceObject | Removes an object from the product interface; currently supported types are expressions and geometry |
SetBuilderVersion | Sets the version of this builder. |
SetUserComments | Sets the user comments on the product interface item passed in |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateAttributesFromPart | Updates the attributes of the product interface items in the part |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ObjectBuilderBuilderVersion Enumeration | Version number of product interface builder |
ObjectBuilderMate Enumeration | An enum representing the settings available for rule checking during creation of mating conditions |
ObjectBuilderWave Enumeration | An enum representing settings available for rule checking during creation of WAVE geomtery and interpart expressions |
Property Detail¶
MateSetting¶
-
ObjectBuilder.
MateSetting
¶ Returns or sets the current rule setting for use during creation of mating conditions
-------------------------------------
Getter Method
Signature
MateSetting
Returns: Return type: NXOpen.Assemblies.ProductInterface.ObjectBuilderMate
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MateSetting
Parameters: mateSetting ( NXOpen.Assemblies.ProductInterface.ObjectBuilderMate
) –New in version NX5.0.0.
License requirements: None.
PartGeometryCopy¶
-
ObjectBuilder.
PartGeometryCopy
¶ Returns the part geometry copy
-------------------------------------
Getter Method
Signature
PartGeometryCopy
Returns: Return type: NXOpen.Features.PartGeometryCopyBuilder
New in version NX9.0.0.
License requirements: None.
WaveSetting¶
-
ObjectBuilder.
WaveSetting
¶ Returns or sets the current rule setting for use during creation of WAVE geomtery and interpart expressions
-------------------------------------
Getter Method
Signature
WaveSetting
Returns: Return type: NXOpen.Assemblies.ProductInterface.ObjectBuilderWave
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WaveSetting
Parameters: waveSetting ( NXOpen.Assemblies.ProductInterface.ObjectBuilderWave
) –New in version NX5.0.0.
License requirements: None.
Method Detail¶
AddProductInterface¶
-
ObjectBuilder.
AddProductInterface
¶ Adds an object to the product interface; currently supported types are expressions and geometry.
If the object already exists, it becomes active.
Signature
AddProductInterface(nxItem)
Parameters: nxItem ( NXOpen.NXObject
) – nx item to be added to the product interfaceReturns: a tuple Return type: A tuple consisting of (prodIntItem, alreadyExisted). prodIntItem is a NXOpen.Assemblies.ProductInterface.InterfaceObject
. the product interface object created or modified alreadyExisted is a bool.New in version NX8.5.1.
License requirements: None.
AddProductInterfaceObject¶
-
ObjectBuilder.
AddProductInterfaceObject
¶ Adds an object to the product interface; currently supported types are expressions and geometry
Signature
AddProductInterfaceObject(nxItem)
Parameters: nxItem ( NXOpen.NXObject
) – nx item to be added to the product interfaceReturns: the product interface object created Return type: NXOpen.Assemblies.ProductInterface.InterfaceObject
New in version NX5.0.0.
License requirements: None.
AddProductInterfaceObject1¶
-
ObjectBuilder.
AddProductInterfaceObject1
¶ Adds an object to the product interface; currently supported types are expressions and geometry
Signature
AddProductInterfaceObject1(nxObject, name, description, reverseDirection)
Parameters: - nxObject (
NXOpen.NXObject
) – Selected object to add - name (str) – User defined name of selected object
- description (str) – User comments of selected object
- reverseDirection (bool) – Flag to specify whether to reverse the direction of the source object
Returns: the product interface object created
Return type: New in version NX9.0.0.
License requirements: None.
- nxObject (
AddProductInterfaceObject2¶
-
ObjectBuilder.
AddProductInterfaceObject2
¶ Adds an object to the product interface; currently supported types are expressions and geometry.
Interface Usage type can be set using this API.
Signature
AddProductInterfaceObject2(nxObject, name, description, reverseDirection, interfaceUsageType)
Parameters: - nxObject (
NXOpen.NXObject
) – Selected object to add - name (str) – User defined name of selected object
- description (str) – User comments of selected object
- reverseDirection (bool) – Flag to specify whether to reverse the direction of the source object
- interfaceUsageType (
NXOpen.Assemblies.ProductInterface.InterfaceObjectInterfaceUsageType
) – Usage type of product interface object
Returns: the product interface object created
Return type: New in version NX12.0.0.
License requirements: None.
- nxObject (
EditProductInterfaceObject¶
-
ObjectBuilder.
EditProductInterfaceObject
¶ Edits a product interface object
Signature
EditProductInterfaceObject(productInterface, nxObject, name, description, reverseDirection)
Parameters: - productInterface (
NXOpen.Assemblies.ProductInterface.InterfaceObject
) – Product interface object to be edited - nxObject (
NXOpen.NXObject
) – Selected object to add - name (str) – User defined name of selected object
- description (str) – User comments of selected object
- reverseDirection (bool) – Flag to specify whether to reverse the direction of the source object
New in version NX9.0.0.
License requirements: None.
- productInterface (
EditProductInterfaceObject1¶
-
ObjectBuilder.
EditProductInterfaceObject1
¶ Edits a product interface object with interface object type .
Interface Usage type can be set using this API.
Signature
EditProductInterfaceObject1(productInterface, nxObject, name, description, reverseDirection, interfaceUsageType)
Parameters: - productInterface (
NXOpen.Assemblies.ProductInterface.InterfaceObject
) – Product interface object to be edited - nxObject (
NXOpen.NXObject
) – Selected object to add - name (str) – User defined name of selected object
- description (str) – User comments of selected object
- reverseDirection (bool) – Flag to specify whether to reverse the direction of the source object
- interfaceUsageType (
NXOpen.Assemblies.ProductInterface.InterfaceObjectInterfaceUsageType
) – Usage type of product interface object
New in version NX12.0.0.
License requirements: None.
- productInterface (
GetBuilderVersion¶
-
ObjectBuilder.
GetBuilderVersion
¶ Gets the version of this builder.
Signature
GetBuilderVersion()
Returns: Return type: NXOpen.Assemblies.ProductInterface.ObjectBuilderBuilderVersion
New in version NX9.0.0.
License requirements: None.
QueryProductInterfaceObjects¶
-
ObjectBuilder.
QueryProductInterfaceObjects
¶ Returns a list of product interface objects in the part
Signature
QueryProductInterfaceObjects(part)
Parameters: part ( NXOpen.NXObject
) – part whose product interface objects have to be queriedReturns: objects in the product interface Return type: list of NXOpen.Assemblies.ProductInterface.InterfaceObject
New in version NX5.0.0.
License requirements: None.
RemoveProductInterfaceObject¶
-
ObjectBuilder.
RemoveProductInterfaceObject
¶ Removes an object from the product interface; currently supported types are expressions and geometry
Signature
RemoveProductInterfaceObject(prodIntItem)
Parameters: prodIntItem ( NXOpen.Assemblies.ProductInterface.InterfaceObject
) – product interface object to be removed from the product interface setNew in version NX5.0.0.
License requirements: None.
SetBuilderVersion¶
-
ObjectBuilder.
SetBuilderVersion
¶ Sets the version of this builder.
Signature
SetBuilderVersion(version)
Parameters: version ( NXOpen.Assemblies.ProductInterface.ObjectBuilderBuilderVersion
) –New in version NX9.0.0.
License requirements: None.
SetUserComments¶
-
ObjectBuilder.
SetUserComments
¶ Sets the user comments on the product interface item passed in
Signature
SetUserComments(prodIntItem, userComments)
Parameters: - prodIntItem (
NXOpen.Assemblies.ProductInterface.InterfaceObject
) – product interface item on which the user comments have to set - userComments (str) – user comments to be set on specified product interface item
New in version NX5.0.0.
License requirements: None.
- prodIntItem (
UpdateAttributesFromPart¶
-
ObjectBuilder.
UpdateAttributesFromPart
¶ Updates the attributes of the product interface items in the part
Signature
UpdateAttributesFromPart(part)
Parameters: part ( NXOpen.NXObject
) – part, product interface objects of which need to have their attributes updatedNew in version NX5.0.0.
License requirements: None.
Validate¶
-
ObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.