ObjectBuilderBuilderVersion Enumeration¶
NXOpen.Assemblies.ProductInterface.ObjectBuilder.BuilderVersion is an alias for NXOpen.Assemblies.ProductInterface.ObjectBuilderBuilderVersion
-
class
NXOpen.Assemblies.ProductInterface.
ObjectBuilderBuilderVersion
¶ Bases:
object
Version number of product interface builder
Enum Members
Enum Member Enum Member Description Original linked feature cannot select the product interface item One linked feature can directly select the product interface item Two product interface builder supports composite curve, composite face and body collector options Three Enables product interface types but used along with the ‘Enable Product Interface Type’ customer default -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-