ObjectBuilderMate Enumeration¶
NXOpen.Assemblies.ProductInterface.ObjectBuilder.Mate is an alias for NXOpen.Assemblies.ProductInterface.ObjectBuilderMate
-
class
NXOpen.Assemblies.ProductInterface.
ObjectBuilderMate
¶ Bases:
object
An enum representing the settings available for rule checking during creation of mating conditions
Enum Members
Enum Member Enum Member Description NoCheck no checking for product interface objects Warn warn user while using non product interface objects Prevent restrict user from using non product interface objects -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-