InterfaceObjectInterfaceUsageType Enumeration¶
NXOpen.Assemblies.ProductInterface.InterfaceObject.InterfaceUsageType is an alias for NXOpen.Assemblies.ProductInterface.InterfaceObjectInterfaceUsageType
-
class
NXOpen.Assemblies.ProductInterface.
InterfaceObjectInterfaceUsageType
¶ Bases:
object
An enum representing product interface usage types
Enum Members
Enum Member Enum Member Description Unknown usage type as unknown Output usage type as output Input usage type as input KeyPerformanceInterface usage type as key performance interface -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-