PartGeometryCopyBuilder Class¶
-
class
NXOpen.Features.
PartGeometryCopyBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.Features.PartGeometryCopyBuilder
builderNew in version NX9.0.0.
Properties¶
Property | Description |
---|---|
InterfaceUsageType | Returns or sets the interface usage type of selected item |
ObjectList | Returns the list of copied objects |
ObjectType | Returns or sets the type of object to be copied |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateSelectionBuilder | Creates a part geometry copy select builder |
Enumerations¶
PartGeometryCopyBuilderType Enumeration | Specifies object types to copy in the part geometry copy block |
Property Detail¶
InterfaceUsageType¶
-
PartGeometryCopyBuilder.
InterfaceUsageType
¶ Returns or sets the interface usage type of selected item
-------------------------------------
Getter Method
Signature
InterfaceUsageType
Returns: Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterfaceUsageType
Parameters: interfaceUsageType (int) – New in version NX12.0.0.
License requirements: gateway (“UG GATEWAY”)
ObjectList¶
-
PartGeometryCopyBuilder.
ObjectList
¶ Returns the list of copied objects
-------------------------------------
Getter Method
Signature
ObjectList
Returns: Return type: NXOpen.Features.PartGeometryCopySelectBuilderList
New in version NX9.0.0.
License requirements: None.
ObjectType¶
-
PartGeometryCopyBuilder.
ObjectType
¶ Returns or sets the type of object to be copied
-------------------------------------
Getter Method
Signature
ObjectType
Returns: Return type: NXOpen.Features.PartGeometryCopyBuilderType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectType
Parameters: objectType ( NXOpen.Features.PartGeometryCopyBuilderType
) –New in version NX9.0.0.
License requirements: gateway (“UG GATEWAY”)
Method Detail¶
CreateSelectionBuilder¶
-
PartGeometryCopyBuilder.
CreateSelectionBuilder
¶ Creates a part geometry copy select builder
Signature
CreateSelectionBuilder(objectType)
Parameters: objectType ( NXOpen.Features.PartGeometryCopyBuilderType
) – Type of object to be copiedReturns: selection builder Return type: NXOpen.Features.PartGeometryCopySelectBuilder
New in version NX9.0.0.
License requirements: None.