PartGeometryCopyBuilderType Enumeration¶
NXOpen.Features.PartGeometryCopyBuilder.Type is an alias for NXOpen.Features.PartGeometryCopyBuilderType
-
class
NXOpen.Features.
PartGeometryCopyBuilderType
¶ Bases:
object
Specifies object types to copy in the part geometry copy block
Enum Members
Enum Member Enum Member Description Automatic An option to select point, datum, sketch, body, and curve feature BodyCollector An option to select bodies via body selection intent BodyObject An option to select body, body-based feature, and body group CurveFeature Curve-based feature Sketch Sketch feature Datum Datum plane, datum axis or datum coordinate system feature Point Point CompositeCurve An option to composite a curve via curve selection intent CompositeFace An option to composite a body via face selection intent Expression Expression Pmi PMI dimension Curve Curve or edge Face Face RoutingObject Routing Object -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-