ReplAsstBuilder Class¶
-
class
NXOpen.GeometricUtilities.
ReplAsstBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.ReplAsstBuilder
.This is the primary data container for Replacement Assistant mapping environment available on editing Linked Body, Linked Face, Extract Body, Extract Face and Mirror Body features. Execute Enter() before invoking any match creation or automatic matching APIs. Call Exit() to exit the mapping environment.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Allowance | Returns or sets the deviation allowance for geometric matching |
MatchList | Returns the list of all Parent Equivalency Map objects |
MatchSheetBoundariesOnly | Returns or sets the automatic matching preference to match sheet boundaries only |
OneToOne | Returns or sets the one to one auto matching preference |
Tag | Returns the Tag for this object. |
UsageInfoList | Returns the list of all Entity Usage Info objects |
Methods¶
Method | Description |
---|---|
CreateEmptyMatch | This is the default creator for a parent equivalency map. |
CreateGeometricMaps | Perform geometric matching. |
CreateInferredMaps | Infer more matches from matches already ‘Accepted’. |
CreateNameBasedMaps | Perform automatic matching based on user-defined object names. |
Enter | Entry and re-entry to the Replacement Assistant mapping environment. |
Exit | Exit the Replacement Assistant mapping environment. |
QueryFeatureOutputUsage | Query the downstream usage of the current feature’s output entities and populate the usageInfoList. |
SetNewParents | Set the source entities for the Replacement Assistant. |
SetProdInt | Set the product interface tag for the Replacement Assistant. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Allowance¶
-
ReplAsstBuilder.
Allowance
¶ Returns or sets the deviation allowance for geometric matching
-------------------------------------
Getter Method
Signature
Allowance
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Allowance
Parameters: allowance (float) – New in version NX6.0.0.
License requirements: None.
MatchList¶
-
ReplAsstBuilder.
MatchList
¶ Returns the list of all Parent Equivalency Map objects
-------------------------------------
Getter Method
Signature
MatchList
Returns: Return type: NXOpen.GeometricUtilities.ParentEquivalencyMapList
New in version NX6.0.0.
License requirements: None.
MatchSheetBoundariesOnly¶
-
ReplAsstBuilder.
MatchSheetBoundariesOnly
¶ Returns or sets the automatic matching preference to match sheet boundaries only
-------------------------------------
Getter Method
Signature
MatchSheetBoundariesOnly
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MatchSheetBoundariesOnly
Parameters: sheetBoundariesOnly (bool) – New in version NX6.0.0.
License requirements: None.
OneToOne¶
-
ReplAsstBuilder.
OneToOne
¶ Returns or sets the one to one auto matching preference
-------------------------------------
Getter Method
Signature
OneToOne
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OneToOne
Parameters: oneToOne (bool) – New in version NX6.0.0.
License requirements: None.
UsageInfoList¶
-
ReplAsstBuilder.
UsageInfoList
¶ Returns the list of all Entity Usage Info objects
-------------------------------------
Getter Method
Signature
UsageInfoList
Returns: Return type: NXOpen.GeometricUtilities.EntityUsageInfoList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
CreateEmptyMatch¶
-
ReplAsstBuilder.
CreateEmptyMatch
¶ This is the default creator for a parent equivalency map.
Signature
CreateEmptyMatch()
Returns: Return type: NXOpen.GeometricUtilities.ParentEquivalencyMap
New in version NX6.0.0.
License requirements: None.
CreateGeometricMaps¶
-
ReplAsstBuilder.
CreateGeometricMaps
¶ Perform geometric matching.
Signature
CreateGeometricMaps()
Returns: new maps created by geometric matching Return type: list of NXOpen.GeometricUtilities.ParentEquivalencyMap
New in version NX6.0.0.
License requirements: None.
CreateInferredMaps¶
-
ReplAsstBuilder.
CreateInferredMaps
¶ Infer more matches from matches already ‘Accepted’.
Add [array_order_guaranteed] annotation for output array when API wrap allows the same.
Signature
CreateInferredMaps()
Returns: new maps created by inferring Return type: list of NXOpen.GeometricUtilities.ParentEquivalencyMap
New in version NX6.0.0.
License requirements: None.
CreateNameBasedMaps¶
-
ReplAsstBuilder.
CreateNameBasedMaps
¶ Perform automatic matching based on user-defined object names.
Signature
CreateNameBasedMaps()
Returns: new maps created by name-based matching Return type: list of NXOpen.GeometricUtilities.ParentEquivalencyMap
New in version NX6.0.0.
License requirements: None.
Enter¶
-
ReplAsstBuilder.
Enter
¶ Entry and re-entry to the Replacement Assistant mapping environment.
This function needs to be executed before invoking any match creation or automatic matching APIs. The matches inferred internally (internal identifier reuse, inherited from parent and siblings) will be populated when this function is executed for the first time after selecting a replacement entity.
Signature
Enter()
New in version NX6.0.0.
License requirements: None.
Exit¶
-
ReplAsstBuilder.
Exit
¶ Exit the Replacement Assistant mapping environment.
Any match creation or automatic matchping API cannot be executed after this function is called.
Signature
Exit()
New in version NX6.0.0.
License requirements: None.
QueryFeatureOutputUsage¶
-
ReplAsstBuilder.
QueryFeatureOutputUsage
¶ Query the downstream usage of the current feature’s output entities and populate the usageInfoList.
This API need be called only ONCE per feature being reparented.
Signature
QueryFeatureOutputUsage()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
SetNewParents¶
-
ReplAsstBuilder.
SetNewParents
¶ Set the source entities for the Replacement Assistant.
If there are matches already created and the body is changed, the matches will be deleted.
Signature
SetNewParents(replacementObjects)
Parameters: replacementObjects (list of NXOpen.DisplayableObject
) – replacement objectsNew in version NX6.0.0.
License requirements: None.
SetProdInt¶
-
ReplAsstBuilder.
SetProdInt
¶ Set the product interface tag for the Replacement Assistant.
Signature
SetProdInt(prodInt)
Parameters: prodInt ( NXOpen.TaggedObject
) –New in version NX11.0.1.
License requirements: None.
Validate¶
-
ReplAsstBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.