ExtractFaceBuilderFaceOptionType Enumeration¶
NXOpen.Features.ExtractFaceBuilder.FaceOptionType is an alias for NXOpen.Features.ExtractFaceBuilderFaceOptionType
-
class
NXOpen.Features.
ExtractFaceBuilderFaceOptionType
¶ Bases:
object
enum for face option type
Enum Members
Enum Member Enum Member Description SingleFace single face type AdjacentFaces adjacent face type AllBodyFaces all faces of body option FaceChain selection intent option -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-