ExtractFaceBuilderFaceSurfaceType Enumeration¶
NXOpen.Features.ExtractFaceBuilder.FaceSurfaceType is an alias for NXOpen.Features.ExtractFaceBuilderFaceSurfaceType
-
class
NXOpen.Features.
ExtractFaceBuilderFaceSurfaceType
¶ Bases:
object
type of resulting surface
Enum Members
Enum Member Enum Member Description SameAsOriginal extracted surface is the same as the original surface PolynomialCubic extracted surface is a cubic polynomial approximation of the original surface GeneralBSurface extracted surface is a B-surface approximation of the original surface -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-