See: Description
Interface | Description |
---|---|
AllAroundVision |
Represents an all-around vision feature
To create or edit an instance of this class, use AllAroundVisionBuilder Created in NX8.5.0 |
AllAroundVisionBuilder |
A
AllAroundVisionBuilder used to create or edit
a vehicle design AllAroundVision feature. |
BaseDataBuilder |
Represents a
BaseDataBuilder . |
BaseDataDriverBuilder |
Represents a
BaseDataDriverBuilder . |
BaseDataImportExportBuilder |
Represents a
BaseDataImportExportBuilder
builder used to import and export expressions from and to a spreadsheet. |
BaseDataLoadingBuilder |
Represents a
BaseDataLoadingBuilder . |
BaseDataLoadingWheelBuilder |
Represents a
BaseDataLoadingWheelBuilder . |
BaseDataPassengerBuilder |
Represents a
BaseDataPassengerBuilder . |
BaseDataWheelBuilder |
Represents a
BaseDataWheelBuilder . |
BumperPendulum |
Represents a bumper pendulum feature
To create or edit an instance of this class, use BumperPendulumBuilder Created in NX8.5.0 |
BumperPendulumBuilder |
Represents a
BumperPendulum builder
To create a new instance of this class, use VehicleDesignCollection.createBumperPendulumBuilder(nxopen.features.vehicledesign.BumperPendulum) Default values. |
CloseRangeBlindVolumeListItemBuilder |
Represents the builder to create blind volume list item used for close range visibility.
|
CloseRangeCameraListItemBuilder |
Represents the builder to create camera list item used for close range visibility.
|
CloseRangeCameraListItemBuilderList |
Represents a list of objects.
|
CloseRangeDemoCylinderListItemBuilder |
Represents the builder to create demo cylinder list item used for close range visibility.
|
CloseRangeDemoCylinderListItemBuilderList |
Represents a list of objects.
|
CloseRangeVisibility |
Represents a close range visibility feature
To create or edit an instance of this class, use CloseRangeVisibilityBuilder Created in NX8.5.0 |
CloseRangeVisibilityBuilder |
The builder to create close range visibility feature.
|
CrashBarrier |
Represents a crash barrier feature
To create or edit an instance of this class, use CrashBarrierBuilder Created in NX8.5.0 |
CrashBarrierBuilder |
Represents a
CrashBarrier builder
to create and edit a vehicle design crash barrier. |
DynamicCurb |
Represents a dynamic curb feature
To create or edit an instance of this class, use DynamicCurbBuilder Created in NX8.5.0 |
DynamicCurbBuilder |
Represents a
DynamicCurb builder
To create a new instance of this class, use VehicleDesignCollection.createDynamicCurbBuilder(nxopen.features.vehicledesign.DynamicCurb) Default values. |
GroundClearance |
Represents a ground clearance feature.
|
GroundClearanceBuilder |
Represents a
GroundClearance builder. |
HeadImpact |
Represents a head impact feature.
|
HeadImpactAPillar |
Represents a head impact a-pillar feature.
|
HeadImpactAPillarBuilder |
Represents a
HeadImpactAPillarBuilder . |
HeadImpactAPillarDetailBuilder |
Represents a
HeadImpactAPillarDetailBuilder . |
HeadImpactAPillarWizardBuilder |
Represents a
HeadImpactAPillarWizardBuilder . |
HeadImpactBPillar |
Represents a head impact b-pillar feature.
|
HeadImpactBPillarBuilder |
Represents a
HeadImpactBPillarBuilder . |
HeadImpactBPillarDetailBuilder |
Represents a
HeadImpactBPillarDetailBuilder . |
HeadImpactBPillarWizardBuilder |
Represents a
HeadImpactBPillarWizardBuilder . |
HeadImpactBuilder |
Represents a
HeadImpactBuilder . |
HeadImpactFrontHeader |
Represents a head impact front header feature.
|
HeadImpactFrontHeaderBuilder |
Represents a
HeadImpactFrontHeaderBuilder . |
HeadImpactFrontHeaderDetailBuilder |
Represents a
HeadImpactFrontHeaderDetailBuilder . |
HeadImpactFrontHeaderWizardBuilder |
Represents a
HeadImpactFrontHeaderWizardBuilder . |
HeadImpactOPillar |
Represents a head impact side rail feature.
|
HeadImpactOPillarBuilder |
Represents a
HeadImpactOPillarBuilder . |
HeadImpactOPillarDetailBuilder |
Represents a
HeadImpactOPillarDetailBuilder . |
HeadImpactOPillarWizardBuilder |
Represents a
HeadImpactOPillarWizardBuilder . |
HeadImpactOtherRail |
Represents a head impact additional side rail feature.
|
HeadImpactOtherRailBuilder |
Represents a
HeadImpactOtherRailBuilder . |
HeadImpactOtherRailDetailBuilder |
Represents a
HeadImpactOtherRailDetailBuilder . |
HeadImpactOtherRailWizardBuilder |
Represents a
HeadImpactOtherRailWizardBuilder . |
HeadImpactRearHeader |
Represents a head impact rear header feature.
|
HeadImpactRearHeaderBuilder |
Represents a
HeadImpactRearHeaderBuilder . |
HeadImpactRearHeaderDetailBuilder |
Represents a
HeadImpactRearHeaderDetailBuilder . |
HeadImpactRearHeaderWizardBuilder |
Represents a
HeadImpactRearHeaderWizardBuilder . |
HeadImpactRPillar |
Represents a head impact rear pillar feature.
|
HeadImpactRPillarBuilder |
Represents a
HeadImpactRPillarBuilder . |
HeadImpactRPillarDetailBuilder |
Represents a
HeadImpactRPillarDetailBuilder . |
HeadImpactRPillarWizardBuilder |
Represents a
HeadImpactRPillarWizardBuilder . |
HeadImpactSideRail |
Represents a head impact side rail feature.
|
HeadImpactSideRailBuilder |
Represents a
HeadImpactSideRailBuilder . |
HeadImpactSideRailDetailBuilder |
Represents a
HeadImpactSideRailDetailBuilder . |
HeadImpactSideRailWizardBuilder |
Represents a
HeadImpactSideRailWizardBuilder . |
HeadImpactUpperRoof |
Represents a head impact upper roof feature.
|
HeadImpactUpperRoofBuilder |
Represents a
HeadImpactUpperRoofBuilder . |
HeadImpactUpperRoofDetailBuilder |
Represents a
HeadImpactUpperRoofDetailBuilder . |
HeadImpactUpperRoofWizardBuilder |
Represents a
HeadImpactUpperRoofWizardBuilder . |
HoodVisibility |
Represents a hood visibility spline feature
To create or edit an instance of this class, use HoodVisibilityBuilder Created in NX6.0.0 |
HoodVisibilityBuilder |
Represents a
HoodVisibility builder
To create a new instance of this class, use VehicleDesignCollection.createHoodVisibilityBuilder(nxopen.features.vehicledesign.HoodVisibility) Default values. |
InnerAngle |
Represents an inner angle feature
To create or edit an instance of this class, use InnerAngleBuilder Created in NX8.5.0 |
InnerAngleBuilder |
Represents a
InnerAngle builder,
used to create or edit inner angle feature. |
Manikin |
Represents a manikin automotive feature
To create or edit an instance of this class, use ManikinBuilder Created in NX7.5.0 |
ManikinBuilder |
Represents a
Manikin builder
To create a new instance of this class, use VehicleDesignCollection.createManikinBuilder(nxopen.features.vehicledesign.Manikin) Default values. |
MirrorCertification |
Represents a mirror certification feature.
|
MirrorCertificationBuilder |
A
MirrorCertificationBuilder used to create or edit
a vehicle design MirrorCertification feature. |
OilPan |
Represents a oil pan feature
To create or edit an instance of this class, use OilPanBuilder Created in NX8.5.0 |
OilPanBuilder |
Represents a
OilPan builder to create and edit a vehicle design oil pan. |
PedestrianProtection |
Represents a pedestrian protection feature
To create or edit an instance of this class, use PedestrianProtectionBuilder Created in NX6.0.0 |
PedestrianProtectionBuilder |
Represents a
PedestrianProtection builder
To create a new instance of this class, use VehicleDesignCollection.createPedestrianProtectionBuilder(nxopen.features.vehicledesign.PedestrianProtection) Default values. |
PendulumPlacementBuilder |
This builder allows you to define the pendulum placement information for bumper pendulum features in vehicle design.
|
ReflectionData |
Represents a reflection data feature
To create or edit an instance of this class, use ReflectionDataBuilder Created in NX6.0.0 |
ReflectionDataBuilder |
Represents a
ReflectionData builder
To create a new instance of this class, use VehicleDesignCollection.createReflectionDataBuilder(nxopen.features.vehicledesign.ReflectionData) Default values. |
SeatBeltAnchorage |
Represents a seat belt anchorage feature
To create or edit an instance of this class, use SeatBeltAnchorageBuilder Created in NX6.0.0 |
SeatBeltAnchorageBuilder |
Represents a
Features.VehicleDesign.SeatBeltAnchorage builder
To create a new instance of this class, use VehicleDesignCollection.createSeatBeltAnchorageBuilder(nxopen.features.vehicledesign.SeatBeltAnchorage) Default values. |
Slope |
Represents a Slope feature
To create or edit an instance of this class, use SlopeBuilder Created in NX8.5.0 |
SlopeBuilder |
The builder to create slope feature.
|
StaticCurb |
Represents a static curb feature
To create or edit an instance of this class, use StaticCurbBuilder Created in NX8.5.0 |
StaticCurbBuilder |
Represents a
StaticCurb builder
used to create or edit static curb feature
To create a new instance of this class, use VehicleDesignCollection.createStaticCurbBuilder(nxopen.features.vehicledesign.StaticCurb) Default values. |
TireEnvelope |
Represents a tire envelope feature
To create or edit an instance of this class, use TireEnvelopeBuilder Created in NX7.5.0 |
TireEnvelopeBuilder |
Represents a builder that is used to edit or create a
TireEnvelope . |
VehicleCoordinateSystem |
Represents a vehicle coordinate system feature
To create or edit an instance of this class, use VehicleCoordinateSystemBuilder Created in NX7.0.0 |
VehicleCoordinateSystemBuilder |
Represents a
VehicleCoordinateSystem builder
To create a new instance of this class, use VehicleDesignCollection.createVehicleCoordinateSystemBuilder(nxopen.features.vehicledesign.VehicleCoordinateSystem) Created in NX7.0.0 |
VisionPlane |
Represents a vision plane feature.
|
VisionPlaneBuilder |
Represents a
VisionPlane builder used to create or edit a Vision Plane. |
WheelCovering |
Represents a wheel covering feature
To create or edit an instance of this class, use WheelCoveringBuilder Created in NX8.5.0 |
WheelCoveringBuilder |
Represents a
WheelCovering
feature builder for wheel covering surface section checking. |
WheelFixing |
Represents a wheel fixing feature
To create or edit an instance of this class, use WheelFixingBuilder Created in NX8.5.0 |
WheelFixingBuilder |
Represents a
WheelFixing builder used to
create or edit a vehicle design wheel fixing. |
WindshieldDatum |
Represents a windshield datum feature.
|
WindshieldDatumBuilder |
Represents a
WindshieldDatum builder used to create or edit a Windshield Datum. |
Class | Description |
---|---|
AllAroundVisionBuilder.Types |
Used to indicate the type of obstructing geometry to use.
|
AllAroundVisionBuilder.WindowTypes |
Used to indicate the type of geometry used to define the window.
|
BaseDataImportExportBuilder.AssignItemNumberData |
This class holds the data returned from
BaseDataImportExportBuilder.assignItemNumber() |
BaseDataImportExportBuilder.AssignItemRevisionData |
This class holds the data returned from
BaseDataImportExportBuilder.assignItemRevision(java.lang.String) |
BaseDataImportExportBuilder.ExportOptions |
This enum represents the option to indicate if the expressions are to be exported to a new item or an existing item in Teamcenter.
|
BaseDataImportExportBuilder.OperateOptions |
This enum represents the import or export operate options
|
BaseDataLoadingBuilder.LoadingType |
This enum represents the vehicle loading types.
|
BaseDataLoadingWheelBuilder.DataDefinitionOptions |
This enum represents the options to define the wheel position.
|
BaseDataPassengerBuilder.SeatDirectionOptions |
This enum represents the options to define the passenger's seat direction type.
|
BaseDataWheelBuilder.PositionDefinitionOptions |
This enum represents the options to define the wheel position.
|
BumperPendulumBuilder.RequirementsControlType |
Represents the requirements control types to define the bumper pendulum.
|
BumperPendulumBuilder.VisualizationType |
Represents the visualization types of the output.
|
CloseRangeCameraListItemBuilder.Types |
This enum represents the camera definition options to define the close range visibility.
|
CloseRangeDemoCylinderListItemBuilder.ValidateTypes |
This enum represents the simple or detailed checking options to validate demo cylinders visibility.
|
CloseRangeVisibilityBuilder.EyePointOffsetTypes |
This enum represents the eye position offset options.
|
CloseRangeVisibilityBuilder.EyePointTypes |
This enum represents the binocular or monocular eye position definition options.
|
CloseRangeVisibilityBuilder.PathPositionTypes |
This enum represents the cylinder path position display options.
|
CloseRangeVisibilityBuilder.PositionMethods |
This enum represents the cylinder position method options.
|
CloseRangeVisibilityBuilder.PositionPaths |
This enum represents the cylinder position path options.
|
CloseRangeVisibilityBuilder.RequirementsControlType |
This enum represents the standard or user defined requirement options.
|
CrashBarrierBuilder.CrossPositionType |
Represents the cross position types.
|
CrashBarrierBuilder.OverlapSideType |
Represents the overlap side types for the front and rear barriers.
|
CrashBarrierBuilder.PositionObjectType |
Represents the position object types.
|
CrashBarrierBuilder.RequirementsControlsControlType |
Represents the requirements control types to define the crash barrier.
|
CrashBarrierBuilder.ShapeType |
Represents the shape types.
|
CrashBarrierBuilder.SideOverlapSideType |
Represents the overlap side types for side barrier.
|
CrashBarrierBuilder.SidePositionType |
Represents the position types for side barrier.
|
DynamicCurbBuilder.MethodType |
Represents the type of inner line to create dynamic curb.
|
DynamicCurbBuilder.PositionType |
Represents the dynamic curb positions.
|
DynamicCurbBuilder.RequirementsControlType |
Represents the requirements control types to define the dynamic curb.
|
DynamicCurbBuilder.VisualizationType |
Represents the visualization types of the output.
|
DynamicCurbBuilder.WheelType |
Represents the type of the wheel size option for dynamic curb.
|
GroundClearanceBuilder.PositionType |
Represents the ground clearance positions.
|
GroundClearanceBuilder.RequirementControls |
This enum represents the standard or user defined requirement options for ground clearance.
|
GroundClearanceBuilder.SectionCurveType |
Represents the type of under axle section curve type to create ground clearace.
|
GroundClearanceBuilder.SurfaceLengthType |
Represents the type of general surface length to create ground clearace.
|
GroundClearanceBuilder.VisualizationTypes |
This enum represents the output definition options.
|
GroundClearanceBuilder.WheelType |
Represents the type of the wheel size option for ground clearance.
|
HeadImpactAPillarDetailBuilder.MeasurementMethodType |
Represents the measurement methods used to position point 1.
|
HeadImpactBuilder.CalculationType |
Represents the calculation types.
|
HeadImpactBuilder.RequirementsControlType |
Represents the requirements control types.
|
InnerAngleBuilder.CalculationMethodType |
Represents the calculation method types to calculate inner angle output.
|
InnerAngleBuilder.RequirementsControlType |
Represents the requirements control types to define the inner angle.
|
InnerAngleBuilder.VisualizationType |
Represents the visualization types of the output.
|
InnerAngleBuilder.WheelSizeType |
Represents the wheel size types to calculate inner angle output.
|
ManikinBuilder.ClassificationType |
the vehicle classification type
|
ManikinBuilder.PositionType |
the vehicle seat position type
|
ManikinBuilder.SAEPercentileType |
the vehicle percentile type
|
ManikinBuilder.StandardType |
the vehicle standard type
|
MirrorCertificationBuilder.DriverSideStandardsType |
Used to indicate the standard for the driver mirror.
|
MirrorCertificationBuilder.EyeFromOptionType |
Used to indicate what part the eye is from.
|
MirrorCertificationBuilder.EyellipsePercentileType |
Used to indicate the eyellipse percentile that is used in mirror certification.
|
MirrorCertificationBuilder.EyeMethodType |
Used to indicate the method to calculate the eye location based on the distance from the eyellipse to the mirror pivot.
|
MirrorCertificationBuilder.EyePointMethodType |
Used to indicate the method to define the eye point.
|
MirrorCertificationBuilder.InsideStandardsType |
Used to indicate the standard for the inside mirror.
|
MirrorCertificationBuilder.InstructionFieldPositionType |
Used to indicate the postion where the instruction field will be.
|
MirrorCertificationBuilder.InstructionFieldsType |
Used to indicate the shape type of the instruction field.
|
MirrorCertificationBuilder.LocationType |
Used to indicate the mirror location.
|
MirrorCertificationBuilder.MirrorOrientationType |
Used to indicate the method to rotate mirror.
|
MirrorCertificationBuilder.MirrorSurfaceType |
Used to indicate the mirror surface type.
|
MirrorCertificationBuilder.PassengerSideStandardsType |
Used to indicate the standard for the passenger mirror.
|
MirrorCertificationBuilder.ShowVisionConeType |
Used to indicate what vision cone will be shown.
|
OilPanBuilder.PositionType |
Represents the oil pan positions.
|
OilPanBuilder.RequirementsControlType |
Represents the requirements control types to define the oil pan.
|
OilPanBuilder.VisualizationType |
Represents the visualization types of the output.
|
PedestrianProtectionBuilder.Font |
Settings for font to create the various output with
|
PedestrianProtectionBuilder.StandardType |
Settings for the type of pedestrian protection standard to use in the study
|
PedestrianProtectionBuilder.TransformMethods |
Settings for the transform method of pedestrian protection active hood system
|
PedestrianProtectionBuilder.Types |
Settings for the type of pedestrian protection impact study
|
PedestrianProtectionBuilder.Wad |
Settings for the start, end and boundary wrap around distance line to create
|
PedestrianProtectionBuilder.Width |
Settings for width to create the various output with
|
PendulumPlacementBuilder.LocationType |
This enum represents the pendulum placement location options.
|
PendulumPlacementBuilder.PendulumProfileType |
This enum represents the pendulum placement profile options.
|
PendulumPlacementBuilder.PositionMethodType |
This enum represents the pendulum placement method options.
|
PendulumPlacementBuilder.SideType |
This enum represents the pendulum placement side options.
|
ReflectionDataBuilder.ResolutionType |
the resolution type
|
SeatBeltAnchorageBuilder.AnchorageLocationTypes |
the seat belt anchorage location type
|
SeatBeltAnchorageBuilder.ATLType |
the show ATL type
|
SeatBeltAnchorageBuilder.LOneLimitType |
the lone limit type
|
SeatBeltAnchorageBuilder.LowerAreaType |
the lower area type
|
SeatBeltAnchorageBuilder.LowerLimitType |
the lower limit type
|
SeatBeltAnchorageBuilder.LTwoLimitType |
the ltwo limit type
|
SeatBeltAnchorageBuilder.RoutingTypes |
the seat belt routing type
|
SeatBeltAnchorageBuilder.SeatPositionTypes |
the seat position type
|
SeatBeltAnchorageBuilder.SeatTypes |
the seat type
|
SeatBeltAnchorageBuilder.StandardTypes |
the standard type
|
SeatBeltAnchorageBuilder.UpperAreaType |
the upper area type
|
SlopeBuilder.PositionType |
Represents the slope positions.
|
SlopeBuilder.RequirementsControlType |
Represents the requirements control types to define the slope.
|
SlopeBuilder.VisualizationType |
Represents the visualization types of the output.
|
SlopeBuilder.WheelSizeType |
Represents the wheel size types to calculate slope output.
|
StaticCurbBuilder.PositionType |
Represents the static curb positions.
|
StaticCurbBuilder.RequirementsControlType |
Represents the requirements control types to define the static curb.
|
StaticCurbBuilder.VisualizationType |
Represents the visualization types of the output.
|
TireEnvelopeBuilder.DriverGraphOption |
Settings to indicate the driver definition to use with the MacPherson Strut suspension template.
|
TireEnvelopeBuilder.EnvelopeOffsetMethod |
Settings to indicate how the offset will be defined.
|
TireEnvelopeBuilder.MotionMethod |
Settings to indicate how the suspension system motion will be defined.
|
TireEnvelopeBuilder.SpindleFileLocationOption |
Settings to indicate the location to select the spindle file.
|
TireEnvelopeBuilder.SuspensionTemplateType |
Settings to indicate the defined suspension template to use.
|
TireEnvelopeBuilder.TireDefinitionOption |
Settings to indicate how the tire profile will be defined.
|
VehicleCoordinateSystemBuilder.Types |
Vehicle Coordinate System type
|
VisionPlaneBuilder.CustomVisionAngle |
Represents the vision angle type to define the Vision Plane.
|
VisionPlaneBuilder.EnumEyeType |
Represents the eye definition type to define the Vision Plane.
|
WheelCoveringBuilder.PositionType |
Represents the wheel covering positions.
|
WheelCoveringBuilder.RequirementsControlType |
Represents the requirements control types to define the wheel covering.
|
WheelCoveringBuilder.SurfacePlaneType |
Represents the type of the surface plane.
|
WheelCoveringBuilder.SurfaceSectionType |
Represents the type of the surface section.
|
WheelFixingBuilder.ObjectPositionType |
Represents the object position used to indicate if the wheel fixing is positioned at the theoretically
widest dimension of the wheel (diameter) or exactly at the wheel geometry of the base data.
|
WheelFixingBuilder.PositionType |
Represents the wheel fixing positions.
|
WheelFixingBuilder.RequirementsControlType |
Represents the requirements control types to define the wheel fixing.
|
WheelFixingBuilder.ShapeType |
Represents the shape used to indicate if the wheel fixing is a block or a circle segment.
|
WheelFixingBuilder.WheelSizeType |
Represents the wheel size used to indicate if the wheel fixing is based on static radius or the diameter of the wheels.
|
WindshieldDatumBuilder.CustomVisionAngle |
Represents the vision angle type to define the Windshield Datum.
|
WindshieldDatumBuilder.EnumEyeType |
Represents the eye definition type to define the Windshield Datum.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.