Interface | Description |
---|---|
ComplexScalarFieldWrapper |
This class defines a complex value that is internally
backed up by a field or two expressions.
|
DisplayPropertiesBuilder | |
ExportData |
Represents data for field export
To create a new instance of this class, use FieldManager.createExportData() Created in NX6.0.0 |
Field |
Represents an Field abstract class.
|
FieldCollection |
Represents a collection of Fields
To obtain an instance of this class, refer to FieldManager Created in NX4.0.0 |
FieldDomain |
Represents the Field Domains.
|
FieldDomainCollection |
Provides methods for manipulating the field domains
To obtain an instance of this class, refer to FieldManager Created in NX4.0.0 |
FieldEvaluator |
Represents a Field Evaluator which can be used to evaluate a
Field . |
FieldExpression |
Represents the Field Expression class.
|
FieldFormula |
Represents the Field Formula class.
|
FieldLink |
Represents the Field Link class.
|
FieldLinksTable |
Represents the Field LinksTable class.
|
FieldManager |
Represents the manager class of the Fields
This manager class gives access to all the fields Field within a part,
as well as the collection of domains FieldDomain . |
FieldReference |
Represents an reference field
A Reference Field exposes data inside of an abstract data store. |
FieldTable |
Represents the Field Table class.
|
FieldVariable |
Represents the Field Variables
A variable is a symbol on whose value a function, polynomial, etc., depends. |
FieldWrapper |
This class defines a value that is internally backed up by a field.
|
ImportData |
Represents data transfer objectst for field import
To create a new instance of this class, use FieldManager.createImportData() Created in NX6.0.0 |
NameVariable |
This class stores the common name and measure for field variables.
|
PathObjects |
Contains objects that define a lattice path
Not a KF builder; see Fields.FieldManager methods to create a Fields.PathObjects. |
PathObjectsList |
Represents a list of objects.
|
ScalarFieldWrapper |
This class defines a scalar value that is internally
backed up by a (optionally scaled) field or an expression.
|
SpatialMap |
Represents the Field Domain Map
A Spatial Map provides a mapping from a field's independent domain into a new domain space. |
SpatialMapBuilder | |
VectorFieldWrapper |
This class defines a vector value that is internally
backed up by a (optionally scaled) field or three expressions.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.