public interface FieldLinksTable extends Field
Field
) defined in terms of tabular data involving
one look-up independent column, an equal number of look-up fields and one or more
dependent variables (see FieldVariable
). This is similar to a table
(see FieldTable
), except instead of the interpolation dependent
values being defined as numerical contants, they are defined by another field. FieldManager
. DisplayableObject.ObjectFont, DisplayableObject.ObjectWidth
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
boolean |
discontinuities()
Returns a flag specifying if the table has discontinuites
License requirements: None. |
void |
editFieldLinksTable(FieldVariable[] indepVarArray,
FieldVariable[] depVarArray,
double[] datapoints,
Field[] linkFieldsArray)
Edit the LinksTable field.
|
void |
setValuesOutsideTableInterpolation(FieldEvaluator.ValuesOutsideTableInterpolationEnum interpolationMethod)
License requirements: None. |
FieldEvaluator.ValuesOutsideTableInterpolationEnum |
valuesOutsideTableInterpolation()
Returns the outside table values interpolation method for linear interpolation
License requirements: None. |
copyAsTableToPart, copyToPart, createCopyInPart, createTableInPart, delete, getDependentVariables, getDescription, getFieldEvaluator, getIdLabel, getIndependentVariables, getSpatialMap, isLocked, isUserField, rename, setDescription, setIdLabel, setSpatialMap, xygraph, xygraph, xygraph, xygraph3DScaleAndReturnPlots, xygraphAndReturnPlots, xygraphArgand, xygraphScaleAndReturnPlots
blank, color, highlight, isBlanked, layer, lineFont, lineWidth, nameLocation, redisplayObject, removeViewDependency, setColor, setLayer, setLineFont, setLineWidth, setNameLocation, unblank, unhighlight
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
void editFieldLinksTable(FieldVariable[] indepVarArray, FieldVariable[] depVarArray, double[] datapoints, Field[] linkFieldsArray) throws NXException, RemoteException
FieldVariable
s
for independent and dependent variables, as well as the new double values and linked fields.
The datapoints and linked fields arrays are row based and number of each must equal the
num_rows. The data_points array represents the values for the first independent value. For example, if
the LinksTable has a domain of txyz, the values in this array are all values of t.
The linked fields array must consist of the fields with independent variables representing the
remaining variables in the independent domain of the LinksTable. For example, if the LinksTable has
a domain of txyz, the independent domain of the fields in this array are all xyz. NULL values are allowed for
linked fields and indicate a discontinuity at the associated value of the first independent variable.
The dependent quantities are determined from the linked fields. The linked fields must have the same
dependent variables as the Linkstable.
indepVarArray
- independent variables to be associated with the fielddepVarArray
- dependent variables of this and all linked fieldsdatapoints
- row based array of double values representing the first independent variable; the number of points should equal the number of rows.linkFieldsArray
- row based array of link field values representing the table; the number of fields should equal the number of rows.NXException
RemoteException
boolean discontinuities() throws NXException, RemoteException
NXException
RemoteException
FieldEvaluator.ValuesOutsideTableInterpolationEnum valuesOutsideTableInterpolation() throws NXException, RemoteException
NXException
RemoteException
void setValuesOutsideTableInterpolation(FieldEvaluator.ValuesOutsideTableInterpolationEnum interpolationMethod) throws NXException, RemoteException
interpolationMethod
- the outside table values interpolation methodNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.